Hello,
I have DM3730 board with ARM_A8 BSP and WinCE 6 R3. I created an image with KITL and VMINI disabled. The build is successfully downled to flash through Ethernet using LAN9221 on board. After booting to the desktop, I ping the board at address 192.168.0.3 from my development PC and get reply. However, when I telnet to the same address, I got the message below:
Connecting To 192.168.0.3...Could not open connection to the host, on port 23: Connect failed
Would anyone please tell me what I am missing? Why does "ping' work but not "telnet"?
Thanks,
Luan