Other Parts Discussed in Thread: TVP7002
We're currently in the evaluation & planning phase of a new project, and are looking at which of development kits will most closely meet our
needs.
Quick system overview-
there are two type boards based on DM8168.
one board:
Need to be able to capture(2 HD 1080p60), encode and transfer to host via ethernet, H.264.
the other board :
Need to be able to receive multi-bitstream (2 HD 1080p60 or 4 1080p30 or 8 D1) from ethernet, decode,display through HDMI.
Thanks!