This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with non-standart YCC8 digital output in interlaced mode - field bit always low (DM368)



Hi!

I'm trying to output 768x576 video via VPBE on dm368

Here is how I config regs:

    unsigned int temp = 0;
    void __iomem *pinmux1    = (void __iomem *) IO_ADDRESS(0x01C40004);
    temp = __raw_readl(pinmux1);  //select VCLKL and HVSYNC
    temp &= ~(0x01 << 22);    //VCLK Enable
    __raw_writel(temp, pinmux1);

__raw_writel(0x38, IO_ADDRESS(SYS_VPSS_CLKCTL)); //clock configured for 29.5 Mhz
    dispc_reg_out(VENC_OSDCLK0, 1);
    dispc_reg_out(VENC_OSDCLK1, 2);
    dispc_reg_out(VENC_DACTST, 0x0);
    
    //YCC8 BT.656
    dispc_reg_out(VENC_CLKCTL, 0x11);
    //OSD Set
    __raw_writel(mode_info->left_margin, IO_ADDRESS(DM365_OSD_REG_BASE + OSD_BASEPX));
    __raw_writel(mode_info->upper_margin + 2,   IO_ADDRESS(DM365_OSD_REG_BASE    + OSD_BASEPY));
    dispc_reg_out(VENC_VIDCTL, 0x6000);
    dispc_reg_out(VENC_DCLKCTL, 0x005);
    dispc_reg_out(VENC_DCLKPTN0, 0x13);    
    dispc_reg_out(VENC_SYNCCTL, 0x400F);
    dispc_reg_out(VENC_VMOD, 0x1251);
    dispc_reg_out(VENC_YCCCTL, 0x1);
    dispc_reg_out(VENC_VDPRO, 0x100);
    dispc_reg_out(VENC_HINT, 0x75F);
    dispc_reg_out(VENC_HSTART, 0x15C);
    dispc_reg_out(VENC_HVALID, 0x600);    
    dispc_reg_out(VENC_VINT, 0x271);
    dispc_reg_out(VENC_VSTART, 0x18);
    dispc_reg_out(VENC_VVALID, 0x120);

I captured data with logic analyzer and discovered that field bit in SAV/EAV code are always zero. But it must be equal zero for 288 lines+vertical blanking and must be equal 1 for another part of frame. Please help, what am I doing wrong?

Here is what I captured:

non-standart 768x576 digital output:

1222.vzu768front2ms.TXT

standart pal 720x576 digital output(works fine):

5277.vzu720front2ms.TXT