Hello.
I'm new to DSP's and I've worked only with MCU's so far, so I'm completely lost and will appreciate any sort of advice.
Apart from processing large amounts of data I need to visualize 4 processed signals at one's and make a very very simple GUI. Can it be done with a TMS320C6657 DSP? Do I need an ARM processor or an MCU apart from C6657? If I can use TMS320C6657 then what is the best way to connect an LCD 7'' 640x480 (with an LCD controller) to the TMDSEVM6657LS evaluation board? I think only EMIF and uPP can potentially be used for that, am I right?
Any help is appreciated,
Alexander.