This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Jelly Bean 4AJ.2.3 Ducati firmware

Hi.

Previous releases of JB for OMAP4 had the firmware name ducati-m3.bin built into the kernel file arch/arm/mach-omap2/remoteproc.c.  Also, the file ducati-m3.bin was included in the tarball device/ti/proprietary-open/omap4/ducati_blaze_tablet.tgz.

Now in the 4AJ.2.3 release, arch/arm/mach-omap2/remoteproc.c specifies the firmware name ducati-m3-core0.xem3.  But the ducati tarball still contains ducati-m3.bin, not ducati-m3-core0.xem3.

I tried renaming the firmware, but the format is not what is expected by the core remoteproc driver.  drivers/remoteproc/remoteproc_core.c generates the error "rproc remoteproc0: Unsupported class: 2".  That's because ducati-m3.bin is ELF class 64 while remoteproc expects ELF class 32.

Where can I obtain ducati-m3-core0.xem3 suitable for 4AJ.2.3?

Regards,

    Steve