Can we use a 14 pin JTAG with the DM81xx devices or must we populate with a 20 pin?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I personally think that it is common for devices with JTAG to be able to use both 14 and 20 pin headers; only the appropriate pinout has to be respected, refer to articles like this one:
http://processors.wiki.ti.com/index.php/JTAG_Connectors
http://processors.wiki.ti.com/index.php/JTAG_Connectors#Pinout
Pages like these in the processors wiki, also let me think that the 14 pin header is an option on DM814x/DM816x:
http://processors.wiki.ti.com/index.php/TI814x-DDR3-Init-U-Boot
http://processors.wiki.ti.com/index.php/TI814x-DDR3-Init-U-Boot_Wordwise_SWleveling
Thank you.
BR
Vladimir