This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure kernel for testing OTG protocols on OMAP4430 PandaBoard?

Hi,

I am new to Linux and try to test OTG protocols (HNP and SRP) on PandaBoard with OMAP4430. Based on OMAP4430 TRM, We can make sure HW supports OTG, but I don't know

1. Is there any OTG build image exist for OMAP4430 or PandaBoard? If any, where to download it?

2. Is there any linux kernel source suite for OMAP4430 OTG test without modifying its source code? If any, where to download it and which defconfig is suite for OMAP4430 Pandaboard? If no, which linux kernel is best for testing OTG on PandaBoard with minimum modification?

Much appreciated!!

-YH