Other Parts Discussed in Thread: SYSCONFIG
hello,
I rebuilt the kernel ,when I use the prebulid filesystem as the nfs,it come to
VFS: Mounted root (nfs filesystem) on device 0:15.
devtmpfs: mounted
Freeing init memory: 232K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udevd (67): /proc/67/oom_adj is deprecated, please use /proc/67/oom_score_adj instead.
Root filesystem already rw, not remounting
Caching udev devnodes
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
Mon Dec 31 10:37:00 UTC 2012
INIT: Entering runlevel: 5
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000001
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00050002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x2d8b6676
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0x019af45e
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM Initialization completed
syslink: disagrees about version of symbol module_layout
FATAL: Error inserting syslink (/lib/modules/2.6.37/kernel/drivers/dsp/syslink.ko): Invalid module format
I don't know how to rebuilt the syslink.ko
thanks
enson