Other Parts Discussed in Thread: TVP7002
Hi, I am confused about the config id H264_DEC_002 in "H264 High Profile Decoder 2.0 on HDVICP2 and Media Controller based platform Data Sheet ".
File above shows that the H264_DEC_002 supports resolutions between 2048 x 2048 and 4096 x 4096, and the example of bbccrowded_i4096x2320_47mbps_IPB_30fps.264 shows that the framerate is up to 30.I want to know how many HDVICP2s are used here,1 or 2? Is H264_DEC_002 something to be configured?
I`m using TI8168 EVM and DVRRDK 3.0. I`m using vdec+vdis demo and the display links are dropped to test the decoder individually. The framerate is about 60 when decoding a 3840x1080 video,and result shows that only one HDVICP is used. However, when decoding 2 3840x1080 videos, the framerate is only 30+ which I think should be 60 because 2 HDVICPs are used here. What limits the framerate in this case?
Thanks,