This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failure of Jffs2 root file system booting

Other Parts Discussed in Thread: OMAPL138

I am using OMAPL138 processor. I flashed Jffs2 image as root file system and trying to boot.  It is booting but giving lot of errors. If I switch off, then next reboot will not happen properly and keep on gives lot of error messages. Can you please suggest how to resolve this issue. I am using 2.6.37 kernel. Also following the steps given in the following link

http://processors.wiki.ti.com/index.php/Booting_Linux_kernel_using_U-Boot.

The jffs2 errors are as follows.

mtd->read(0x744 bytes from 0xc1e0bc) returned ECC error
mtd->read(0x630 bytes from 0xc1c1d0) returned ECC error
mtd->read(0x674 bytes from 0xc1c18c) returned ECC error
mtd->read(0x630 bytes from 0xc1a9d0) returned ECC error
mtd->read(0x674 bytes from 0xc1a98c) returned ECC error
mtd->read(0x44 bytes from 0xc1e100) returned ECC error
mtd->read(0x7bc bytes from 0xc1e044) returned ECC error
mtd->read(0x800 bytes from 0xc1e000) returned ECC error
mtd->read(0x6ec bytes from 0xc1c114) returned ECC error
mtd->read(0x730 bytes from 0xc1c0d0) returned ECC error
mtd->read(0x6ec bytes from 0xc1a914) returned ECC error
mtd->read(0x730 bytes from 0xc1a8d0) returned ECC error
JFFS2 notice: (645) jffs2_get_inode_nodes: Node header CRC failed at 0x0b0854. {df67,5121,5121df67,5121df67}
mtd->read(0x44 bytes from 0xc1e044) returned ECC error
JFFS2 notice: (645) jffs2_get_inode_nodes: Node header CRC failed at 0x0b0918. {0000,0000,000000f2,5121e061}
JFFS2 warning: (645) jffs2_do_read_inode_internal: no data nodes found for ino #234
Returned error for crccheck of ino #234. Expect badness...
JFFS2 notice: (645) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0b0a94.
JFFS2 warning: (645) jffs2_do_read_inode_internal: no data nodes found for ino #235
Returned error for crccheck of ino #235. Expect badness...