This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

file system boot failure on dm8168

Hi all

i use dm8168 dvrrdk 2.8 packages, usually the board boot ok,

but when i shut down the power when the jffs2 file system is mounting,

sometimes it seems jffs2 broken,or i just power on/off frequently it also appears.

the system will blocked follow message printed

SysLink version : 2.10.02.17
SysLink module created on Date:Dec 18 2012 Time:14:16:27
Trace enabled
Trace SetFailureReason enabled
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Jan 22 2013 17:53:19
VPSS_FVID2: create handle is NULL
VPSS_SYSTEM: failed to create handle
VPSS_CORE : failed to init system
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
ti81xxfb: Unknown symbol vps_grpx_get_ctrl (err 0)
ti81xxfb: Unknown symbol vps_grpx_get_num_grpx (err 0)
ti81xxhdmi: Unknown symbol TI81xx_un_register_display_panel (err 0)
ti81xxhdmi: Unknown symbol TI81xx_register_display_panel (err 0)

when i reflash the jffs2 file system, it works well

Is this jffs2 system features then?how to solve this problem ?

best regards

xavier