Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Changes in U-Boot Code for Custom AM335x Board

Hi,

I am trying to build a board around AM335x. I have used the AMM335x-EVM configuration and got a new PCB. Till now I am able to see 'C' on serial port.

When I am trying to load BSP on to SD card and try to boot the board, it is trying to read the configuration ID from EEPROM on the board and not booting the OS.

But its a blank EEPROM on my board.

Can anyone please suggest me what modifications do I need to do in the U-boot code to get solve this.?

Is there any documentation available for this SDK-Linux.?

Thanks & Regards

Sai Viswanadh Chukka

  • Hi Sai,

    There is a lot of documentation for the AM335x Linux SDK, all of which can be found through the Sitara AM335x Portal.
    Here is a link to the Sitara Linux Software Developer’s Guide and also to the AM335x Platform Support Package User's Guide.
    Here is also a link to the AM335x U-Boot User's Guide - if your custom board has a boot switch (just like SW3 on the AM335x EVM), you can check the Boot Switch Settings section to see how to tell the ROM code to boot from SD card.

    If your custom board doesn't have a boot switch, then you need to check if the sysboot pins are hardwired and what is their boot configuration. For more information please refer to Table 26-7. SYSBOOT Configuration Pins (page 4058) from the AM335x Technical Reference Manual. You may also want to check the AM335x GP EVM Board Design Files.

    Best regards,
    Miroslav

  • Hi Miroslav,

    Thanks for the information.  To avoid  eerprom checks, I modified evm.c file.

    Commented few parts of read_eeprom()  function and hard coded the AM335x 15x15 Baseboard EEPROM Data as given in EVM AM335x Hardware user guide.

    Now we are facing some more error.  Here are those

    ------------------------------------------
    CCCCCCCC
    U-Boot SPL 2011.09 (Mar 08 2013 - 19:17:19)
    Texas Instruments Revision detection unimplemented
            Board name   : A33515BB     <-- we kept few printfs to confirm
            Board version: 1.0A
            Board serial : 03134P160001
            Board config : SKU#01
    
            Board name   : A33515BB
            Board version: 1.0A
            Board serial : 03134P160001
            Board config : SKU#01
    
    No daughter card present
            Profile configured
    OMAP SD/MMC: 0
    mmc_send_cmd: timedout waiting for cmddis!
    ** Can't read from device 0 **
    spl: fat register err - -1
    ### ERROR ### Please RESET the board ###
    -------------------------------------------

    I have attached the evm.c file.

    /*
     * evm.c
     *
     * Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/
     *
     * This program is free software; you can redistribute it and/or
     * modify it under the terms of the GNU General Public License as
     * published by the Free Software Foundation version 2.
     *
     * This program is distributed "as is" WITHOUT ANY WARRANTY of any
     * kind, whether express or implied; without even the implied warranty
     * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
     * GNU General Public License for more details.
     */
    
    #include <common.h>
    #include <asm/cache.h>
    #include <asm/omap_common.h>
    #include <asm/io.h>
    #include <asm/gpio.h>
    #include <asm/arch/cpu.h>
    #include <asm/arch/ddr_defs.h>
    #include <asm/arch/hardware.h>
    #include <asm/arch/mmc_host_def.h>
    #include <asm/arch/sys_proto.h>
    #include <asm/arch/mem.h>
    #include <asm/arch/nand.h>
    #include <asm/arch/clock.h>
    #include <asm/arch/gpio.h>
    #include <linux/mtd/nand.h>
    #include <nand.h>
    #include <net.h>
    #include <miiphy.h>
    #include <netdev.h>
    #include <spi_flash.h>
    #include "common_def.h"
    #include "pmic.h"
    #include "tps65217.h"
    #include <i2c.h>
    #include <serial.h>
    
    DECLARE_GLOBAL_DATA_PTR;
    
    /* UART Defines */
    #define UART_SYSCFG_OFFSET	(0x54)
    #define UART_SYSSTS_OFFSET	(0x58)
    
    #define UART_RESET		(0x1 << 1)
    #define UART_CLK_RUNNING_MASK	0x1
    #define UART_SMART_IDLE_EN	(0x1 << 0x3)
    
    /* Timer Defines */
    #define TSICR_REG		0x54
    #define TIOCP_CFG_REG		0x10
    #define TCLR_REG		0x38
    
    /* DDR defines */
    #define MDDR_SEL_DDR2		0xefffffff		/* IOs set for DDR2-STL Mode */
    #define CKE_NORMAL_OP		0x00000001		/* Normal Op:CKE controlled by EMIF */
    #define GATELVL_INIT_MODE_SEL	0x1	/* Selects a starting ratio value based
    					on DATA0/1_REG_PHY_GATELVL_INIT_RATIO_0
    					value programmed by the user */
    #define WRLVL_INIT_MODE_SEL	0x1	/* Selects a starting ratio value based
    					on DATA0/1_REG_PHY_WRLVL_INIT_RATIO_0
    					value programmed by the user */
    
    /* CPLD registers */
    #define CFG_REG			0x10
    
    /*
     * I2C Address of various board
     */
    #define I2C_BASE_BOARD_ADDR	0x50
    #define I2C_DAUGHTER_BOARD_ADDR 0x51
    #define I2C_LCD_BOARD_ADDR	0x52
    
    #define I2C_CPLD_ADDR		0x35
    
    /* RGMII mode define */
    #define RGMII_MODE_ENABLE	0xA
    #define RMII_MODE_ENABLE	0x5
    #define MII_MODE_ENABLE		0x0
    
    /* TLK110 PHY registers */
    #define TLK110_COARSEGAIN_REG	0x00A3
    #define TLK110_LPFHPF_REG	0x00AC
    #define TLK110_SPAREANALOG_REG	0x00B9
    #define TLK110_VRCR_REG		0x00D0
    #define TLK110_SETFFE_REG	(unsigned char)0x0107
    #define TLK110_FTSP_REG		(unsigned char)0x0154
    #define TLK110_ALFATPIDL_REG	0x002A
    #define TLK110_PSCOEF21_REG	0x0096
    #define TLK110_PSCOEF3_REG	0x0097
    #define TLK110_ALFAFACTOR1_REG	0x002C
    #define TLK110_ALFAFACTOR2_REG	0x0023
    #define TLK110_CFGPS_REG	0x0095
    #define TLK110_FTSPTXGAIN_REG	(unsigned char)0x0150
    #define TLK110_SWSCR3_REG	0x000B
    #define TLK110_SCFALLBACK_REG	0x0040
    #define TLK110_PHYRCR_REG	0x001F
    
    /* TLK110 register writes values */
    #define TLK110_COARSEGAIN_VAL	0x0000
    #define TLK110_LPFHPF_VAL	0x8000
    #define TLK110_SPAREANALOG_VAL	0x0000
    #define TLK110_VRCR_VAL		0x0008
    #define TLK110_SETFFE_VAL	0x0605
    #define TLK110_FTSP_VAL		0x0255
    #define TLK110_ALFATPIDL_VAL	0x7998
    #define TLK110_PSCOEF21_VAL	0x3A20
    #define TLK110_PSCOEF3_VAL	0x003F
    #define TLK110_ALFAFACTOR1_VAL	0xFF80
    #define TLK110_ALFAFACTOR2_VAL	0x021C
    #define TLK110_CFGPS_VAL	0x0000
    #define TLK110_FTSPTXGAIN_VAL	0x6A88
    #define TLK110_SWSCR3_VAL	0x0000
    #define TLK110_SCFALLBACK_VAL	0xC11D
    #define TLK110_PHYRCR_VAL	0x4000
    #define TLK110_PHYIDR1		0x2000
    #define TLK110_PHYIDR2		0xA201
    
    #define NO_OF_MAC_ADDR          3
    #define ETH_ALEN		6
    
    #define RTC_KICK0_REG		0x6c
    #define RTC_KICK1_REG		0x70
    #define RTC_OSC_REG		0x54
    
    struct am335x_baseboard_id {
    	unsigned int  magic;
    	char name[8];
    	char version[4];
    	char serial[12];
    	char config[32];
    	char mac_addr[NO_OF_MAC_ADDR][ETH_ALEN];
    };
    
    static struct am335x_baseboard_id __attribute__((section (".data"))) header;
    extern void cpsw_eth_set_mac_addr(const u_int8_t *addr);
    static
    unsigned char __attribute__((section (".data"))) daughter_board_connected = 1;
    static volatile int __attribute__((section (".data"))) board_id = SK_BOARD;
    
    /* GPIO base address table */
    static const struct gpio_bank gpio_bank_am335x[4] = {
    	{ (void *)AM335X_GPIO0_BASE, METHOD_GPIO_24XX },
    	{ (void *)AM335X_GPIO1_BASE, METHOD_GPIO_24XX },
    	{ (void *)AM335X_GPIO2_BASE, METHOD_GPIO_24XX },
    	{ (void *)AM335X_GPIO3_BASE, METHOD_GPIO_24XX },
    };
    const struct gpio_bank *const omap_gpio_bank = gpio_bank_am335x;
    
    /*
     * dram_init:
     * At this point we have initialized the i2c bus and can read the
     * EEPROM which will tell us what board and revision we are on.
     */
    int dram_init(void)
    {
    	gd->ram_size = PHYS_DRAM_1_SIZE;
    
    	return 0;
    }
    
    void dram_init_banksize (void)
    {
    	/* Fill up board info */
    	gd->bd->bi_dram[0].start = PHYS_DRAM_1;
    	gd->bd->bi_dram[0].size = PHYS_DRAM_1_SIZE;
    }
    
    #ifdef CONFIG_SPL_BUILD
    static void Data_Macro_Config_ddr2(int dataMacroNum)
    {
            u32 BaseAddrOffset = 0x00;;
    
            if (dataMacroNum == 1)
                    BaseAddrOffset = 0xA4;
    
            writel(((DDR2_RD_DQS<<30)|(DDR2_RD_DQS<<20)
                            |(DDR2_RD_DQS<<10)|(DDR2_RD_DQS<<0)),
                            (DATA0_RD_DQS_SLAVE_RATIO_0 + BaseAddrOffset));
            writel(DDR2_RD_DQS>>2, (DATA0_RD_DQS_SLAVE_RATIO_1 + BaseAddrOffset));
            writel(((DDR2_WR_DQS<<30)|(DDR2_WR_DQS<<20)
                            |(DDR2_WR_DQS<<10)|(DDR2_WR_DQS<<0)),
                            (DATA0_WR_DQS_SLAVE_RATIO_0 + BaseAddrOffset));
            writel(DDR2_WR_DQS>>2, (DATA0_WR_DQS_SLAVE_RATIO_1 + BaseAddrOffset));
            writel(((DDR2_PHY_WRLVL<<30)|(DDR2_PHY_WRLVL<<20)
                            |(DDR2_PHY_WRLVL<<10)|(DDR2_PHY_WRLVL<<0)),
                            (DATA0_WRLVL_INIT_RATIO_0 + BaseAddrOffset));
            writel(DDR2_PHY_WRLVL>>2, (DATA0_WRLVL_INIT_RATIO_1 + BaseAddrOffset));
            writel(((DDR2_PHY_GATELVL<<30)|(DDR2_PHY_GATELVL<<20)
                            |(DDR2_PHY_GATELVL<<10)|(DDR2_PHY_GATELVL<<0)),
                            (DATA0_GATELVL_INIT_RATIO_0 + BaseAddrOffset));
            writel(DDR2_PHY_GATELVL>>2,
                            (DATA0_GATELVL_INIT_RATIO_1 + BaseAddrOffset));
            writel(((DDR2_PHY_FIFO_WE<<30)|(DDR2_PHY_FIFO_WE<<20)
                            |(DDR2_PHY_FIFO_WE<<10)|(DDR2_PHY_FIFO_WE<<0)),
                            (DATA0_FIFO_WE_SLAVE_RATIO_0 + BaseAddrOffset));
            writel(DDR2_PHY_FIFO_WE>>2,
                            (DATA0_FIFO_WE_SLAVE_RATIO_1 + BaseAddrOffset));
            writel(((DDR2_PHY_WR_DATA<<30)|(DDR2_PHY_WR_DATA<<20)
                            |(DDR2_PHY_WR_DATA<<10)|(DDR2_PHY_WR_DATA<<0)),
                            (DATA0_WR_DATA_SLAVE_RATIO_0 + BaseAddrOffset));
            writel(DDR2_PHY_WR_DATA>>2,
                            (DATA0_WR_DATA_SLAVE_RATIO_1 + BaseAddrOffset));
            writel(DDR2_PHY_DLL_LOCK_DIFF,
                            (DATA0_DLL_LOCK_DIFF_0 + BaseAddrOffset));
    }
    
    static void config_vtp(void)
    {
            writel(readl(VTP0_CTRL_REG) | VTP_CTRL_ENABLE, VTP0_CTRL_REG);
            writel(readl(VTP0_CTRL_REG) & (~VTP_CTRL_START_EN), VTP0_CTRL_REG);
            writel(readl(VTP0_CTRL_REG) | VTP_CTRL_START_EN, VTP0_CTRL_REG);
    
            /* Poll for READY */
            while ((readl(VTP0_CTRL_REG) & VTP_CTRL_READY) != VTP_CTRL_READY);
    }
    
    static void phy_config_cmd(void)
    {
    	writel(DDR3_RATIO, CMD0_CTRL_SLAVE_RATIO_0);
    	writel(DDR3_INVERT_CLKOUT, CMD0_INVERT_CLKOUT_0);
    	writel(DDR3_RATIO, CMD1_CTRL_SLAVE_RATIO_0);
    	writel(DDR3_INVERT_CLKOUT, CMD1_INVERT_CLKOUT_0);
    	writel(DDR3_RATIO, CMD2_CTRL_SLAVE_RATIO_0);
    	writel(DDR3_INVERT_CLKOUT, CMD2_INVERT_CLKOUT_0);
    }
    
    static void phy_config_data(void)
    {
    
    	writel(DDR3_RD_DQS, DATA0_RD_DQS_SLAVE_RATIO_0);
    	writel(DDR3_WR_DQS, DATA0_WR_DQS_SLAVE_RATIO_0);
    	writel(DDR3_PHY_FIFO_WE, DATA0_FIFO_WE_SLAVE_RATIO_0);
    	writel(DDR3_PHY_WR_DATA, DATA0_WR_DATA_SLAVE_RATIO_0);
    
    	writel(DDR3_RD_DQS, DATA1_RD_DQS_SLAVE_RATIO_0);
    	writel(DDR3_WR_DQS, DATA1_WR_DQS_SLAVE_RATIO_0);
    	writel(DDR3_PHY_FIFO_WE, DATA1_FIFO_WE_SLAVE_RATIO_0);
    	writel(DDR3_PHY_WR_DATA, DATA1_WR_DATA_SLAVE_RATIO_0);
    }
    
    static void config_emif_ddr3(void)
    {
    	/*Program EMIF0 CFG Registers*/
    	writel(DDR3_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_1);
    	writel(DDR3_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_1_SHADOW);
    	writel(DDR3_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_2);
    	writel(DDR3_EMIF_TIM1, EMIF4_0_SDRAM_TIM_1);
    	writel(DDR3_EMIF_TIM1, EMIF4_0_SDRAM_TIM_1_SHADOW);
    	writel(DDR3_EMIF_TIM2, EMIF4_0_SDRAM_TIM_2);
    	writel(DDR3_EMIF_TIM2, EMIF4_0_SDRAM_TIM_2_SHADOW);
    	writel(DDR3_EMIF_TIM3, EMIF4_0_SDRAM_TIM_3);
    	writel(DDR3_EMIF_TIM3, EMIF4_0_SDRAM_TIM_3_SHADOW);
    
    
    	writel(DDR3_EMIF_SDREF, EMIF4_0_SDRAM_REF_CTRL);
    	writel(DDR3_EMIF_SDREF, EMIF4_0_SDRAM_REF_CTRL_SHADOW);
    	writel(DDR3_ZQ_CFG, EMIF0_0_ZQ_CONFIG);
    
    	writel(DDR3_EMIF_SDCFG, EMIF4_0_SDRAM_CONFIG);
    
    }
    
    static void config_am335x_ddr3(void)
    {
    	enable_ddr3_clocks();
    
    	config_vtp();
    
    	phy_config_cmd();
    	phy_config_data();
    
    	/* set IO control registers */
    	writel(DDR3_IOCTRL_VALUE, DDR_CMD0_IOCTRL);
    	writel(DDR3_IOCTRL_VALUE, DDR_CMD1_IOCTRL);
    	writel(DDR3_IOCTRL_VALUE, DDR_CMD2_IOCTRL);
    	writel(DDR3_IOCTRL_VALUE, DDR_DATA0_IOCTRL);
    	writel(DDR3_IOCTRL_VALUE, DDR_DATA1_IOCTRL);
    
    	/* IOs set for DDR3 */
    	writel(readl(DDR_IO_CTRL) & MDDR_SEL_DDR2, DDR_IO_CTRL);
    	/* CKE controlled by EMIF/DDR_PHY */
    	writel(readl(DDR_CKE_CTRL) | CKE_NORMAL_OP, DDR_CKE_CTRL);
    
    	config_emif_ddr3();
    
    }
    
    static void Cmd_Macro_Config_ddr2(void)
    {
    	writel(DDR2_RATIO, CMD0_CTRL_SLAVE_RATIO_0);
    	writel(DDR2_CMD_FORCE, CMD0_CTRL_SLAVE_FORCE_0);
    	writel(DDR2_CMD_DELAY, CMD0_CTRL_SLAVE_DELAY_0);
    	writel(DDR2_DLL_LOCK_DIFF, CMD0_DLL_LOCK_DIFF_0);
    	writel(DDR2_INVERT_CLKOUT, CMD0_INVERT_CLKOUT_0);
    
    	writel(DDR2_RATIO, CMD1_CTRL_SLAVE_RATIO_0);
    	writel(DDR2_CMD_FORCE, CMD1_CTRL_SLAVE_FORCE_0);
    	writel(DDR2_CMD_DELAY, CMD1_CTRL_SLAVE_DELAY_0);
    	writel(DDR2_DLL_LOCK_DIFF, CMD1_DLL_LOCK_DIFF_0);
    	writel(DDR2_INVERT_CLKOUT, CMD1_INVERT_CLKOUT_0);
    
    	writel(DDR2_RATIO, CMD2_CTRL_SLAVE_RATIO_0);
    	writel(DDR2_CMD_FORCE, CMD2_CTRL_SLAVE_FORCE_0);
    	writel(DDR2_CMD_DELAY, CMD2_CTRL_SLAVE_DELAY_0);
    	writel(DDR2_DLL_LOCK_DIFF, CMD2_DLL_LOCK_DIFF_0);
    	writel(DDR2_INVERT_CLKOUT, CMD2_INVERT_CLKOUT_0);
    }
    
    static void config_emif_ddr2(void)
    {
    	u32 i;
    
    	/*Program EMIF0 CFG Registers*/
    	writel(DDR2_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_1);
    	writel(DDR2_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_1_SHADOW);
    	writel(DDR2_EMIF_READ_LATENCY, EMIF4_0_DDR_PHY_CTRL_2);
    	writel(DDR2_EMIF_TIM1, EMIF4_0_SDRAM_TIM_1);
    	writel(DDR2_EMIF_TIM1, EMIF4_0_SDRAM_TIM_1_SHADOW);
    	writel(DDR2_EMIF_TIM2, EMIF4_0_SDRAM_TIM_2);
    	writel(DDR2_EMIF_TIM2, EMIF4_0_SDRAM_TIM_2_SHADOW);
    	writel(DDR2_EMIF_TIM3, EMIF4_0_SDRAM_TIM_3);
    	writel(DDR2_EMIF_TIM3, EMIF4_0_SDRAM_TIM_3_SHADOW);
    
    	writel(DDR2_EMIF_SDCFG, EMIF4_0_SDRAM_CONFIG);
    	writel(DDR2_EMIF_SDCFG, EMIF4_0_SDRAM_CONFIG2);
    
    	/* writel(DDR2_EMIF_SDMGT, EMIF0_0_SDRAM_MGMT_CTRL);
    	writel(DDR2_EMIF_SDMGT, EMIF0_0_SDRAM_MGMT_CTRL_SHD); */
    	writel(DDR2_EMIF_SDREF1, EMIF4_0_SDRAM_REF_CTRL);
    	writel(DDR2_EMIF_SDREF1, EMIF4_0_SDRAM_REF_CTRL_SHADOW);
    
    	for (i = 0; i < 5000; i++) {
    
    	}
    
    	/* writel(DDR2_EMIF_SDMGT, EMIF0_0_SDRAM_MGMT_CTRL);
    	writel(DDR2_EMIF_SDMGT, EMIF0_0_SDRAM_MGMT_CTRL_SHD); */
    	writel(DDR2_EMIF_SDREF2, EMIF4_0_SDRAM_REF_CTRL);
    	writel(DDR2_EMIF_SDREF2, EMIF4_0_SDRAM_REF_CTRL_SHADOW);
    
    	writel(DDR2_EMIF_SDCFG, EMIF4_0_SDRAM_CONFIG);
    	writel(DDR2_EMIF_SDCFG, EMIF4_0_SDRAM_CONFIG2);
    }
    
    /*  void DDR2_EMIF_Config(void); */
    static void config_am335x_ddr2(void)
    {
    	int data_macro_0 = 0;
    	int data_macro_1 = 1;
    
    	enable_ddr2_clocks();
    
    	config_vtp();
    
    	Cmd_Macro_Config_ddr2();
    
    	Data_Macro_Config_ddr2(data_macro_0);
    	Data_Macro_Config_ddr2(data_macro_1);
    
    	writel(DDR2_PHY_RANK0_DELAY, DATA0_RANK0_DELAYS_0);
    	writel(DDR2_PHY_RANK0_DELAY, DATA1_RANK0_DELAYS_0);
    
    	writel(DDR2_IOCTRL_VALUE, DDR_CMD0_IOCTRL);
    	writel(DDR2_IOCTRL_VALUE, DDR_CMD1_IOCTRL);
    	writel(DDR2_IOCTRL_VALUE, DDR_CMD2_IOCTRL);
    	writel(DDR2_IOCTRL_VALUE, DDR_DATA0_IOCTRL);
    	writel(DDR2_IOCTRL_VALUE, DDR_DATA1_IOCTRL);
    
    	writel(readl(DDR_IO_CTRL) & MDDR_SEL_DDR2, DDR_IO_CTRL);
    	writel(readl(DDR_CKE_CTRL) | CKE_NORMAL_OP, DDR_CKE_CTRL);
    
    	config_emif_ddr2();
    }
    
    static void init_timer(void)
    {
    	/* Reset the Timer */
    	writel(0x2, (DM_TIMER2_BASE + TSICR_REG));
    
    	/* Wait until the reset is done */
    	while (readl(DM_TIMER2_BASE + TIOCP_CFG_REG) & 1);
    
    	/* Start the Timer */
    	writel(0x1, (DM_TIMER2_BASE + TCLR_REG));
    }
    
    static void rtc32k_enable(void)
    {
    	/* Unlock the rtc's registers */
    	writel(0x83e70b13, (AM335X_RTC_BASE + RTC_KICK0_REG));
    	writel(0x95a4f1e0, (AM335X_RTC_BASE + RTC_KICK1_REG));
    
    	/* Enable the RTC 32K OSC */
    	writel(0x48, (AM335X_RTC_BASE + RTC_OSC_REG));
    }
    #endif
    
    /*
     * Read header information from EEPROM into global structure.
     */
    int read_eeprom(void)
    {
            /* Check if baseboard eeprom is available */ // Added by Vish, 07/03/2013
    /*	u_int32_t i,j;
    	unsigned int  magic;
    	char name[8];
    	char version[4];
    	char serial[12];
    	char config[32];
    	char mac_addr[NO_OF_MAC_ADDR][ETH_ALEN];*/
    
            header.magic = 0xEE3355AA; 
    //	header.name  =  "A33515BB";
    	header.name[7]='B';
    	header.name[6]='B';
    	header.name[5]='5';
    	header.name[4]='1';
    	header.name[3]='5';
    	header.name[2]='3';
    	header.name[1]='3';
    	header.name[0]='A';
    
    //	header.serial =  "03134P160001";
            header.version[3] = 'A';    header.version[2] = '0';     header.version[1] = '.';        header.version[0] = '1';   
    
            header.serial[11] = '1';     header.serial[10] = '0';    header.serial[9] =  '0';    
            header.serial[8] =  '0';     header.serial[7] =  '6';    header.serial[6] =  '1';    
            header.serial[5] =  'P';     header.serial[4] =  '4';    header.serial[3] =  '3';    
            header.serial[2] =  '1';     header.serial[1] =  '3';    header.serial[0] =  '0';
    
    //	header.config = "SKU#01";
    	header.config[5] = '1';	
    	header.config[4] = '0';	
    	header.config[3] = '#';	
    	header.config[2] = 'U';	
    	header.config[1] = 'K';	
    	header.config[0] = 'S';	
    
    //	header.mac_addr[NO_OF_MAC_ADDR][ETH_ALEN];        
    
    /* // Commented the following to avoid EEPROM Reading. Added by Vish, 07/03/2013
    	if (i2c_probe(I2C_BASE_BOARD_ADDR)) {
    		printf("Could not probe the EEPROM; something fundamentally "
    			"wrong on the I2C bus.\n");
    		return 1;
    	}
    
    	// read the eeprom using i2c 
    	if (i2c_read(I2C_BASE_BOARD_ADDR, 0, 2, (uchar *)&header,
    							sizeof(header))) {
    		printf("Could not read the EEPROM; something fundamentally"
    			" wrong on the I2C bus.\n");
    		return 1;
    	}
    
    	if (header.magic != 0xEE3355AA) {
    		// read the eeprom using i2c again, but use only a 1 byte address //
    		if (i2c_read(I2C_BASE_BOARD_ADDR, 0, 1, (uchar *)&header,
    								sizeof(header))) {
    			printf("Could not read the EEPROM; something fundamentally"
    				" wrong on the I2C bus.\n");
    			return 1;
    		}
    
    		if (header.magic != 0xEE3355AA) {
    			printf("Incorrect magic number in EEPROM\n");
    			return 1;
    		}
    	debug("\tBoard version: %.4s\n", header.version);
    	debug("\tBoard serial : %.12s\n", header.serial);
    	debug("\tBoard config : %.6s\n\n", header.config);
    	}*/
    		if (header.magic != 0xEE3355AA) {
    			printf("Incorrect magic number in EEPROM\n");
    			return 1;
    		}
    	printf("\tBoard name   : %.8s\n", header.name);
    	printf("\tBoard version: %.4s\n", header.version);
    	printf("\tBoard serial : %.12s\n", header.serial);
    	printf("\tBoard config : %.6s\n\n", header.config);
            printf("First Trail....\n"); //Added by Vish, 07/03/2013
    	return 0;
    }
    
    #if defined(CONFIG_SPL_BUILD) && defined(CONFIG_SPL_BOARD_INIT)
    
    /**
     * tps65217_reg_read() - Generic function that can read a TPS65217 register
     * @src_reg:          Source register address
     * @src_val:          Address of destination variable
     */
    
    unsigned char tps65217_reg_read(uchar src_reg, uchar *src_val)
    {
    	if (i2c_read(TPS65217_CHIP_PM, src_reg, 1, src_val, 1))
    		return 1;
    	return 0;
    }
    
    /**
     *  tps65217_reg_write() - Generic function that can write a TPS65217 PMIC
     *                         register or bit field regardless of protection
     *                         level.
     *
     *  @prot_level:        Register password protection.
     *                      use PROT_LEVEL_NONE, PROT_LEVEL_1, or PROT_LEVEL_2
     *  @dest_reg:          Register address to write.
     *  @dest_val:          Value to write.
     *  @mask:              Bit mask (8 bits) to be applied.  Function will only
     *                      change bits that are set in the bit mask.
     *
     *  @return:            0 for success, 1 for failure.
     */
    int tps65217_reg_write(uchar prot_level, uchar dest_reg,
            uchar dest_val, uchar mask)
    {
            uchar read_val;
            uchar xor_reg;
    
            /* if we are affecting only a bit field, read dest_reg and apply the mask */
            if (mask != MASK_ALL_BITS) {
                    if (i2c_read(TPS65217_CHIP_PM, dest_reg, 1, &read_val, 1))
                            return 1;
                    read_val &= (~mask);
                    read_val |= (dest_val & mask);
                    dest_val = read_val;
            }
    
            if (prot_level > 0) {
                    xor_reg = dest_reg ^ PASSWORD_UNLOCK;
                    if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
                            return 1;
            }
    
            if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
                    return 1;
    
            if (prot_level == PROT_LEVEL_2) {
                    if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
                            return 1;
    
                    if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
                            return 1;
            }
    
            return 0;
    }
    
    /**
     *  tps65217_voltage_update() - Controls output voltage setting for the DCDC1,
     *       DCDC2, or DCDC3 control registers in the PMIC.
     *
     *  @dc_cntrl_reg:      DCDC Control Register address.
     *                      Must be DEFDCDC1, DEFDCDC2, or DEFDCDC3.
     *  @volt_sel:          Register value to set.  See PMIC TRM for value set.
     *
     *  @return:            0 for success, 1 for failure.
     */
    int tps65217_voltage_update(unsigned char dc_cntrl_reg, unsigned char volt_sel)
    {
            if ((dc_cntrl_reg != DEFDCDC1) && (dc_cntrl_reg != DEFDCDC2)
                    && (dc_cntrl_reg != DEFDCDC3))
                    return 1;
    
            /* set voltage level */
            if (tps65217_reg_write(PROT_LEVEL_2, dc_cntrl_reg, volt_sel, MASK_ALL_BITS))
                    return 1;
    
            /* set GO bit to initiate voltage transition */
            if (tps65217_reg_write(PROT_LEVEL_2, DEFSLEW, DCDC_GO, DCDC_GO))
                    return 1;
    
            return 0;
    }
    
    /*
     * voltage switching for MPU frequency switching.
     * @module = mpu - 0, core - 1
     * @vddx_op_vol_sel = vdd voltage to set
     */
    
    #define MPU	0
    #define CORE	1
    
    int voltage_update(unsigned int module, unsigned char vddx_op_vol_sel)
    {
    	uchar buf[4];
    	unsigned int reg_offset;
    
    	if(module == MPU)
    		reg_offset = PMIC_VDD1_OP_REG;
    	else
    		reg_offset = PMIC_VDD2_OP_REG;
    
    	/* Select VDDx OP   */
    	if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
    		return 1;
    
    	buf[0] &= ~PMIC_OP_REG_CMD_MASK;
    
    	if (i2c_write(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
    		return 1;
    
    	/* Configure VDDx OP  Voltage */
    	if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
    		return 1;
    
    	buf[0] &= ~PMIC_OP_REG_SEL_MASK;
    	buf[0] |= vddx_op_vol_sel;
    
    	if (i2c_write(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
    		return 1;
    
    	if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
    		return 1;
    
    	if ((buf[0] & PMIC_OP_REG_SEL_MASK ) != vddx_op_vol_sel)
    		return 1;
    
    	return 0;
    }
    
    void spl_board_init(void)
    {
    	uchar pmic_status_reg;
    
    	/* init board_id, configure muxes */
    	board_init();
    
    	if (!strncmp("A335BONE", header.name, 8)) {
    		/* BeagleBone PMIC Code */
    		if (i2c_probe(TPS65217_CHIP_PM))
    			return;
    
    		if (tps65217_reg_read(STATUS, &pmic_status_reg))
    			return;
    
    		/* Increase USB current limit to 1300mA */
    		if (tps65217_reg_write(PROT_LEVEL_NONE, POWER_PATH,
    				       USB_INPUT_CUR_LIMIT_1300MA,
    				       USB_INPUT_CUR_LIMIT_MASK))
    			printf("tps65217_reg_write failure\n");
    
    		/* Only perform PMIC configurations if board rev > A1 */
    		if (!strncmp(header.version, "00A1", 4))
    			return;
    
    		/* Set DCDC2 (MPU) voltage to 1.275V */
    		if (tps65217_voltage_update(DEFDCDC2,
    					     DCDC_VOLT_SEL_1275MV)) {
    			printf("tps65217_voltage_update failure\n");
    			return;
    		}
    
    		/* Set LDO3, LDO4 output voltage to 3.3V */
    		if (tps65217_reg_write(PROT_LEVEL_2, DEFLS1,
    				       LDO_VOLTAGE_OUT_3_3, LDO_MASK))
    			printf("tps65217_reg_write failure\n");
    
    		if (tps65217_reg_write(PROT_LEVEL_2, DEFLS2,
    				       LDO_VOLTAGE_OUT_3_3, LDO_MASK))
    			printf("tps65217_reg_write failure\n");
    
    		if (!(pmic_status_reg & PWR_SRC_AC_BITMASK)) {
    			printf("No AC power, disabling frequency switch\n");
    			return;
    		}
    
    		/* Set MPU Frequency to 720MHz */
    		mpu_pll_config(MPUPLL_M_720);
    	} else {
    		uchar buf[4];
    		/*
    		 * EVM PMIC code.  All boards currently want an MPU voltage
    		 * of 1.2625V and CORE voltage of 1.1375V to operate at
    		 * 720MHz.
    		 */
    		if (i2c_probe(PMIC_CTRL_I2C_ADDR))
    			return;
    
    		/* VDD1/2 voltage selection register access by control i/f */
    		if (i2c_read(PMIC_CTRL_I2C_ADDR, PMIC_DEVCTRL_REG, 1, buf, 1))
    			return;
    
    		buf[0] |= PMIC_DEVCTRL_REG_SR_CTL_I2C_SEL_CTL_I2C;
    
    		if (i2c_write(PMIC_CTRL_I2C_ADDR, PMIC_DEVCTRL_REG, 1, buf, 1))
    			return;
    
    		if (!voltage_update(MPU, PMIC_OP_REG_SEL_1_2_6) &&
    				!voltage_update(CORE, PMIC_OP_REG_SEL_1_1_3))
    			/* Frequency switching for OPP 120 */
    	 		mpu_pll_config(MPUPLL_M_720);
    	}
    }
    #endif
    
    #define GPIO_DDR_VTT_EN		7
    /*
     * early system init of muxing and clocks.
     */
    void s_init(void)
    {
    	/* Can be removed as A8 comes up with L2 enabled */
    	l2_cache_enable();
    
    	/* WDT1 is already running when the bootloader gets control
    	 * Disable it to avoid "random" resets
    	 */
    	writel(0xAAAA, WDT_WSPR);
    	while(readl(WDT_WWPS) != 0x0);
    	writel(0x5555, WDT_WSPR);
    	while(readl(WDT_WWPS) != 0x0);
    
    #ifdef CONFIG_SPL_BUILD
    	/* Setup the PLLs and the clocks for the peripherals */
    	pll_init();
    
    	/* Enable RTC32K clock */
    	rtc32k_enable();
    
    	/* UART softreset */
    	u32 regVal;
    	u32 uart_base = DEFAULT_UART_BASE;
    
    	enable_uart0_pin_mux();
    	/* IA Motor Control Board has default console on UART3*/
    	/* XXX: This is before we've probed / set board_id */
    	if (board_id == IA_BOARD) {
    		uart_base = UART3_BASE;
    	}
    
    	regVal = readl(uart_base + UART_SYSCFG_OFFSET);
    	regVal |= UART_RESET;
    	writel(regVal, (uart_base + UART_SYSCFG_OFFSET) );
    	while ((readl(uart_base + UART_SYSSTS_OFFSET) &
    			UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK);
    
    	/* Disable smart idle */
    	regVal = readl((uart_base + UART_SYSCFG_OFFSET));
    	regVal |= UART_SMART_IDLE_EN;
    	writel(regVal, (uart_base + UART_SYSCFG_OFFSET));
    
    	/* Initialize the Timer */
    	init_timer();
    
    	preloader_console_init();
    
    	enable_i2c0_pin_mux();
    
    	i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
    
    	if (read_eeprom()) {
    		printf("read_eeprom() failure. continuing with ddr3\n");
    	}
    
    	u32 is_ddr3 = 0;
    	if (!strncmp("A335X_SK", header.name, 8)) {
    		is_ddr3 = 1;
    
    		/*
    		 * EVM SK 1.2A and later use gpio0_7 to enable DDR3.
    		 * This is safe enough to do on older revs.
    		 */
    		enable_gpio0_7_pin_mux();
    		gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en");
    		gpio_direction_output(GPIO_DDR_VTT_EN, 1);
    	}
    
    	if(is_ddr3 == 1){
    		ddr_pll_config(303);
    		config_am335x_ddr3();
    	}
    	else {
    		ddr_pll_config(266);
    		config_am335x_ddr2();
    	}
    
    #endif
    }
    
    static void detect_daughter_board(void)
    {
    	/* Check if daughter board is conneted */
    		printf("No daughter card present\n");
    		daughter_board_connected = 0;
    		return;
    	
    /*	if (i2c_probe(I2C_DAUGHTER_BOARD_ADDR)) { //Commented on 07-03-13 for EVM trails, Added by Vish
    		printf("No daughter card present\n");
    		return;
    	} else {
    		printf("Found a daughter card connected\n");
    		daughter_board_connected = 1;
    	}*/
    }
    
    static unsigned char profile = PROFILE_0;
    static void detect_daughter_board_profile(void)
    {
    	unsigned short val;
    
    //	if (i2c_probe(I2C_CPLD_ADDR))
    //		return;
    
    //	if (i2c_read(I2C_CPLD_ADDR, CFG_REG, 1, (unsigned char *)(&val), 2))
    //		return;
             val = 0x03;
        
    	profile = 0x00; //1 << (val & 0x7);
    	printf("\tProfile configured\n");
    
    }
    
    /*
     * Basic board specific setup
     */
    #ifndef CONFIG_SPL_BUILD
    int board_evm_init(void)
    {
    	/* mach type passed to kernel */
    	if (board_id == IA_BOARD)
    		gd->bd->bi_arch_number = MACH_TYPE_TIAM335IAEVM;
    	else
    		gd->bd->bi_arch_number = MACH_TYPE_TIAM335EVM;
    
    	/* address of boot parameters */
    	gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100;
    
    	return 0;
    }
    #endif
    
    #if 0
    struct serial_device *default_serial_console(void)
    {
    
    	if (board_id != IA_BOARD) {
    		return &eserial1_device;	/* UART0 */
    	} else {
    		return &eserial4_device;	/* UART3 */
    	}
    }
    #endif
    
    int board_init(void)
    {
    	/* Configure the i2c0 pin mux */
    	enable_i2c0_pin_mux();
    
    	i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
    
    	if (read_eeprom())
    		goto err_out;
    
    	detect_daughter_board();
    
    	if (!strncmp("SKU#01", header.config, 6)) {
    		board_id = GP_BOARD;
    		detect_daughter_board_profile();
    	} else if (!strncmp("SKU#02", header.config, 6)) {
    		board_id = IA_BOARD;
    		detect_daughter_board_profile();
    	} else if (!strncmp("SKU#03", header.config, 6)) {
    		board_id = IPP_BOARD;
    	} else if (!strncmp("A335BONE", header.name, 8)) {
    		board_id = BONE_BOARD;
    		profile = 1;	/* profile 0 is internally considered as 1 */
    		daughter_board_connected = 0;
    	} else if (!strncmp("A335X_SK", header.name, 8)) {
    		board_id = SK_BOARD;
    		profile = 1;	/* profile 0 is internally considered as 1 */
    		daughter_board_connected = 0;
    	} else {
    		printf("Did not find a recognized configuration, "
    			"assuming General purpose EVM in Profile 0 with "
    			"Daughter board\n");
    		board_id = GP_BOARD;
    		profile = 1;	/* profile 0 is internally considered as 1 */
    		daughter_board_connected = 1;
    	}
    
    	configure_evm_pin_mux(board_id, header.version, profile, daughter_board_connected);
    
    #ifndef CONFIG_SPL_BUILD
    
            printf("Before evm init 1\n");        //
    	board_evm_init();
            printf("after evm init 1\n");        
    #endif
    
    
            printf("Before gpmc init 1 \n");        
    	gpmc_init();
            printf("After gpmc init 1\n");        
    	return 0;
    
    err_out:
    	/*
    	 * When we cannot use the EEPROM to determine what board we
    	 * are we assume BeagleBone currently as we have not yet
    	 * programmed the EEPROMs.
    	 */
            printf("In err_out \n");
    	board_id = BONE_BOARD;
    	profile = 1;	/* profile 0 is internally considered as 1 */
    	daughter_board_connected = 1;
    	configure_evm_pin_mux(board_id, header.version, profile, daughter_board_connected);
    
    #ifndef CONFIG_SPL_BUILD
            printf("Before evm init 2\n");        
    	board_evm_init();
            printf("after evm init 2\n");        
    
    #endif
            printf("Before gpmc init 2 \n");        
    	gpmc_init();
            printf("After gpmc init 2\n");        
    	return 0;
    }
    int misc_init_r(void)
    {
    #ifdef DEBUG
    	unsigned int cntr;
    	unsigned char *valPtr;
    
    	debug("EVM Configuration - ");
    	debug("\tBoard id %x, profile %x, db %d\n", board_id, profile,
    						daughter_board_connected);
    	debug("Base Board EEPROM Data\n");
    	valPtr = (unsigned char *)&header;
    	for(cntr = 0; cntr < sizeof(header); cntr++) {
    		if(cntr % 16 == 0)
    			debug("\n0x%02x :", cntr);
    		debug(" 0x%02x", (unsigned int)valPtr[cntr]);
    	}
    	debug("\n\n");
    
    	debug("Board identification from EEPROM contents:\n");
    	debug("\tBoard name   : %.8s\n", header.name);
    	debug("\tBoard version: %.4s\n", header.version);
    	debug("\tBoard serial : %.12s\n", header.serial);
    	debug("\tBoard config : %.6s\n\n", header.config);
    #endif
    	return 0;
    }
    
    #ifdef BOARD_LATE_INIT
    int board_late_init(void)
    {
    	if (board_id == IA_BOARD) {
    		/*
    		* SPI bus number is switched to in case Industrial Automation
    		* motor control EVM.
    		*/
    		setenv("spi_bus_no", "1");
    		/* Change console to tty03 for IA Motor Control EVM */
    		setenv("console", "ttyO3,115200n8");
    	}
    
    	return 0;
    }
    #endif
    
    #ifdef CONFIG_DRIVER_TI_CPSW
    /* TODO : Check for the board specific PHY */
    static void evm_phy_init(char *name, int addr)
    {
    	unsigned short val;
    	unsigned int cntr = 0;
    	unsigned short phyid1, phyid2;
    	int bone_pre_a3 = 0;
    
    	if (board_id == BONE_BOARD && (!strncmp(header.version, "00A1", 4) ||
    		    !strncmp(header.version, "00A2", 4)))
    		bone_pre_a3 = 1;
    
    	/*
    	 * This is done as a workaround to support TLK110 rev1.0 PHYs.
    	 * We can only perform these reads on these PHYs (currently
    	 * only found on the IA EVM).
    	 */
    	if ((miiphy_read(name, addr, MII_PHYSID1, &phyid1) != 0) ||
    			(miiphy_read(name, addr, MII_PHYSID2, &phyid2) != 0))
    		return;
    
    	if ((phyid1 == TLK110_PHYIDR1) && (phyid2 == TLK110_PHYIDR2)) {
    		miiphy_read(name, addr, TLK110_COARSEGAIN_REG, &val);
    		val |= TLK110_COARSEGAIN_VAL;
    		miiphy_write(name, addr, TLK110_COARSEGAIN_REG, val);
    
    		miiphy_read(name, addr, TLK110_LPFHPF_REG, &val);
    		val |= TLK110_LPFHPF_VAL;
    		miiphy_write(name, addr, TLK110_LPFHPF_REG, val);
    
    		miiphy_read(name, addr, TLK110_SPAREANALOG_REG, &val);
    		val |= TLK110_SPAREANALOG_VAL;
    		miiphy_write(name, addr, TLK110_SPAREANALOG_REG, val);
    
    		miiphy_read(name, addr, TLK110_VRCR_REG, &val);
    		val |= TLK110_VRCR_VAL;
    		miiphy_write(name, addr, TLK110_VRCR_REG, val);
    
    		miiphy_read(name, addr, TLK110_SETFFE_REG, &val);
    		val |= TLK110_SETFFE_VAL;
    		miiphy_write(name, addr, TLK110_SETFFE_REG, val);
    
    		miiphy_read(name, addr, TLK110_FTSP_REG, &val);
    		val |= TLK110_FTSP_VAL;
    		miiphy_write(name, addr, TLK110_FTSP_REG, val);
    
    		miiphy_read(name, addr, TLK110_ALFATPIDL_REG, &val);
    		val |= TLK110_ALFATPIDL_VAL;
    		miiphy_write(name, addr, TLK110_ALFATPIDL_REG, val);
    
    		miiphy_read(name, addr, TLK110_PSCOEF21_REG, &val);
    		val |= TLK110_PSCOEF21_VAL;
    		miiphy_write(name, addr, TLK110_PSCOEF21_REG, val);
    
    		miiphy_read(name, addr, TLK110_PSCOEF3_REG, &val);
    		val |= TLK110_PSCOEF3_VAL;
    		miiphy_write(name, addr, TLK110_PSCOEF3_REG, val);
    
    		miiphy_read(name, addr, TLK110_ALFAFACTOR1_REG, &val);
    		val |= TLK110_ALFAFACTOR1_VAL;
    		miiphy_write(name, addr, TLK110_ALFAFACTOR1_REG, val);
    
    		miiphy_read(name, addr, TLK110_ALFAFACTOR2_REG, &val);
    		val |= TLK110_ALFAFACTOR2_VAL;
    		miiphy_write(name, addr, TLK110_ALFAFACTOR2_REG, val);
    
    		miiphy_read(name, addr, TLK110_CFGPS_REG, &val);
    		val |= TLK110_CFGPS_VAL;
    		miiphy_write(name, addr, TLK110_CFGPS_REG, val);
    
    		miiphy_read(name, addr, TLK110_FTSPTXGAIN_REG, &val);
    		val |= TLK110_FTSPTXGAIN_VAL;
    		miiphy_write(name, addr, TLK110_FTSPTXGAIN_REG, val);
    
    		miiphy_read(name, addr, TLK110_SWSCR3_REG, &val);
    		val |= TLK110_SWSCR3_VAL;
    		miiphy_write(name, addr, TLK110_SWSCR3_REG, val);
    
    		miiphy_read(name, addr, TLK110_SCFALLBACK_REG, &val);
    		val |= TLK110_SCFALLBACK_VAL;
    		miiphy_write(name, addr, TLK110_SCFALLBACK_REG, val);
    
    		miiphy_read(name, addr, TLK110_PHYRCR_REG, &val);
    		val |= TLK110_PHYRCR_VAL;
    		miiphy_write(name, addr, TLK110_PHYRCR_REG, val);
    	}
    
    	/* Enable Autonegotiation */
    	if (miiphy_read(name, addr, MII_BMCR, &val) != 0) {
    		printf("failed to read bmcr\n");
    		return;
    	}
    
    	if (bone_pre_a3) {
    		val &= ~(BMCR_FULLDPLX | BMCR_ANENABLE | BMCR_SPEED100);
    		val |= BMCR_FULLDPLX;
    	} else
    		val |= BMCR_FULLDPLX | BMCR_ANENABLE | BMCR_SPEED100;
    
    	if (miiphy_write(name, addr, MII_BMCR, val) != 0) {
    		printf("failed to write bmcr\n");
    		return;
    	}
    	miiphy_read(name, addr, MII_BMCR, &val);
    
    	/*
    	 * The 1.0 revisions of the GP board don't have functional
    	 * gigabit ethernet so we need to disable advertising.
    	 */
    	if (board_id == GP_BOARD && !strncmp(header.version, "1.0", 3)) {
    		miiphy_read(name, addr, MII_CTRL1000, &val);
    		val &= ~PHY_1000BTCR_1000FD;
    		val &= ~PHY_1000BTCR_1000HD;
    		miiphy_write(name, addr, MII_CTRL1000, val);
    		miiphy_read(name, addr, MII_CTRL1000, &val);
    	}
    
    	/* Setup general advertisement */
    	if (miiphy_read(name, addr, MII_ADVERTISE, &val) != 0) {
    		printf("failed to read anar\n");
    		return;
    	}
    
    	if (bone_pre_a3)
    		val |= (LPA_10HALF | LPA_10FULL);
    	else
    		val |= (LPA_10HALF | LPA_10FULL | LPA_100HALF | LPA_100FULL);
    
    	if (miiphy_write(name, addr, MII_ADVERTISE, val) != 0) {
    		printf("failed to write anar\n");
    		return;
    	}
    	miiphy_read(name, addr, MII_ADVERTISE, &val);
    
    	/* Restart auto negotiation*/
    	miiphy_read(name, addr, MII_BMCR, &val);
    	val |= BMCR_ANRESTART;
    	miiphy_write(name, addr, MII_BMCR, val);
    
    	/*check AutoNegotiate complete - it can take upto 3 secs*/
    	do {
    		udelay(40000);
    		cntr++;
    		if (!miiphy_read(name, addr, MII_BMSR, &val)) {
    			if (val & BMSR_ANEGCOMPLETE)
    				break;
    		}
    	} while (cntr < 250);
    
    	if (cntr >= 250)
    		printf("Auto Negotitation failed for port %d\n", addr);
    
    	return;
    }
    
    static void cpsw_control(int enabled)
    {
    	/* nothing for now */
    	/* TODO : VTP was here before */
    	return;
    }
    
    static struct cpsw_slave_data cpsw_slaves[] = {
    	{
    		.slave_reg_ofs	= 0x208,
    		.sliver_reg_ofs	= 0xd80,
    		.phy_id		= 0,
    	},
    	{
    		.slave_reg_ofs	= 0x308,
    		.sliver_reg_ofs	= 0xdc0,
    		.phy_id		= 1,
    	},
    };
    
    static struct cpsw_platform_data cpsw_data = {
    	.mdio_base		= AM335X_CPSW_MDIO_BASE,
    	.cpsw_base		= AM335X_CPSW_BASE,
    	.mdio_div		= 0xff,
    	.channels		= 8,
    	.cpdma_reg_ofs		= 0x800,
    	.slaves			= 2,
    	.slave_data		= cpsw_slaves,
    	.ale_reg_ofs		= 0xd00,
    	.ale_entries		= 1024,
    	.host_port_reg_ofs	= 0x108,
    	.hw_stats_reg_ofs	= 0x900,
    	.mac_control		= (1 << 5) /* MIIEN */,
    	.control		= cpsw_control,
    	.phy_init		= evm_phy_init,
    	.gigabit_en		= 1,
    	.host_port_num		= 0,
    	.version		= CPSW_CTRL_VERSION_2,
    };
    
    int board_eth_init(bd_t *bis)
    {
    	uint8_t mac_addr[6];
    	uint32_t mac_hi, mac_lo;
    	u_int32_t i;
    
    	if (!eth_getenv_enetaddr("ethaddr", mac_addr)) {
    		debug("<ethaddr> not set. Reading from E-fuse\n");
    		/* try reading mac address from efuse */
    		mac_lo = readl(MAC_ID0_LO);
    		mac_hi = readl(MAC_ID0_HI);
    		mac_addr[0] = mac_hi & 0xFF;
    		mac_addr[1] = (mac_hi & 0xFF00) >> 8;
    		mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
    		mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
    		mac_addr[4] = mac_lo & 0xFF;
    		mac_addr[5] = (mac_lo & 0xFF00) >> 8;
    
    		if (!is_valid_ether_addr(mac_addr)) {
    			debug("Did not find a valid mac address in e-fuse. "
    					"Trying the one present in EEPROM\n");
    
    			for (i = 0; i < ETH_ALEN; i++)
    				mac_addr[i] = header.mac_addr[0][i];
    		}
    
    		if (is_valid_ether_addr(mac_addr))
    			eth_setenv_enetaddr("ethaddr", mac_addr);
    		else {
    			printf("Caution: Using hardcoded mac address. "
    				"Set <ethaddr> variable to overcome this.\n");
    		}
    	}
    
    	if (board_id == BONE_BOARD) {
    		/* For beaglebone > Rev A2 , enable MII mode, for others enable RMII */
    		if (!strncmp(header.version, "00A1", 4) ||
    		    !strncmp(header.version, "00A2", 4))
    			writel(RMII_MODE_ENABLE, MAC_MII_SEL);
    		else
    			writel(MII_MODE_ENABLE, MAC_MII_SEL);
    		/* No gigabit */
    		cpsw_data.gigabit_en = 0;
    	} else if (board_id == IA_BOARD) {
    		cpsw_slaves[0].phy_id = 30;
    		cpsw_slaves[1].phy_id = 0;
    		/* No gigabit */
    		cpsw_data.gigabit_en = 0;
    	} else {
    		/* set mii mode to rgmii in in device configure register */
    		writel(RGMII_MODE_ENABLE, MAC_MII_SEL);
    	}
    
    	/* GP EVM 1.0 (A, B) does not have functional gigabit */
    	if (board_id == GP_BOARD && !strncmp(header.version, "1.0", 3))
    		cpsw_data.gigabit_en = 0;
    
    	return cpsw_register(&cpsw_data);
    }
    #endif
    
    #ifndef CONFIG_SPL_BUILD
    #ifdef CONFIG_GENERIC_MMC
    int board_mmc_init(bd_t *bis)
    {
    	omap_mmc_init(0);
    	omap_mmc_init(1);
    	return 0;
    }
    #endif
    
    #ifdef CONFIG_NAND_TI81XX
    /******************************************************************************
     * Command to switch between NAND HW and SW ecc
     *****************************************************************************/
    extern void ti81xx_nand_switch_ecc(nand_ecc_modes_t hardware, int32_t mode);
    static int do_switch_ecc(cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[])
    {
    	int type = 0;
    	if (argc < 2)
    		goto usage;
    
    	if (strncmp(argv[1], "hw", 2) == 0) {
    		if (argc == 3)
    			type = simple_strtoul(argv[2], NULL, 10);
    		ti81xx_nand_switch_ecc(NAND_ECC_HW, type);
    	}
    	else if (strncmp(argv[1], "sw", 2) == 0)
    		ti81xx_nand_switch_ecc(NAND_ECC_SOFT, 0);
    	else
    		goto usage;
    
    	return 0;
    
    usage:
    	printf("Usage: nandecc %s\n", cmdtp->usage);
    	return 1;
    }
    
    U_BOOT_CMD(
    	nandecc, 3, 1,	do_switch_ecc,
    	"Switch NAND ECC calculation algorithm b/w hardware and software",
    	"[sw|hw <hw_type>] \n"
    	"   [sw|hw]- Switch b/w hardware(hw) & software(sw) ecc algorithm\n"
    	"   hw_type- 0 for Hamming code\n"
    	"            1 for bch4\n"
    	"            2 for bch8\n"
    	"            3 for bch16\n"
    );
    
    #endif /* CONFIG_NAND_TI81XX */
    #endif /* CONFIG_SPL_BUILD */
    

    Please suggest how can I move further and boot my board.

    Thanks & Regards

    Sai Viswanadh Chukka