Other Parts Discussed in Thread: TMS320C5505
Guys,
Is there any QFP form TMS320C5505?because it's not easy for me on soldering BGA, testing if the connection is properly soldered,
Thanks for helping
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C5505
Guys,
Is there any QFP form TMS320C5505?because it's not easy for me on soldering BGA, testing if the connection is properly soldered,
Thanks for helping
Hi,
There are no QFP packages for C5505.
C5505 DSP is only available in BGA - 0.65mm pitch
Similarly C5515 - BGA with 0.65mm pitch
C5535 - BGA with 0.8mm pitch
To allow debugging on prototype boards its best to escape all signals from the package balls so you have access to them.
Regards,
Mark
I see, I'll put header for every signal pins, any idea on how to solder it manually at home it's very tight for 0.65mm pitch and 196 pins....
can I use heat gun or microwave oven ?