OMAPL138 Champs,
I am trying to determine how to best terminate my unused RTC_ALARM/UART2_CTS/GP0[8]/DEEPSLEEP ball F4 on the OMAPL138
According to section 1.5.10 Pin Multiplexing Control Registers (PINMUX0-PINMUX19) of the technical reference manual (TRM) the default state of this ball (i.e. PINMUX0 = 0x0) will be DEEPSLEEP which is an input. It is also part of CP[0] which will default to an internal pull up according to 11.5.23 Pullup/Pulldown Select Register (PUPD_SEL) in the TRM.
The Schematic checklist and the Section 2.9 Unused Pin Configurations in the Data Sheet only state the following. "RTC_ALARM May be used as GPIO or other peripheral function" This is fairly unclear.
Thanks!