Other Parts Discussed in Thread: OMAP-L138
Hi,
I am trying to write a simple MessageQ application but with no success. This is my environment:
Board: OMAP-L138 EVM (DA850, LogicPD)
ARM: Angstrom Linux
Host: Ubuntu 10.04
Sys/Bios: 6.34.04
SysLink: 2.21.01
IPC: 1.25.01
XDCTools: 3.24.05
Running examples/ex02_messageq works without any problems. Now I tried to set up a simple application from scratch. This is what I've done:
config.bld:
var SR_0 = {
name: "SR_0", space: "data", access: "RWX",
base: 0xC2000000, len: 0x10000,
comment: "SR#0 Memory (64 KB)"
};
var SR_1 = {
name: "SR_1", space: "data", access: "RWX",
base: 0xC2010000, len: 0x20000,
comment: "SR#1 Memory (128 KB)"
};
Build.platformTable["ti.platforms.evmOMAPL138:dsp"] = {
externalMemoryMap: [
[ SR_0.name, SR_0 ],
[ SR_1.name, SR_1 ],
[ "DSP_PROG", {
name: "DSP_PROG", space: "code/data", access: "RWX",
base: 0xC3000000, len: 0x800000,
comment: "DSP Program Memory (8 MB)"
}]
],
codeMemory: "DSP_PROG",
dataMemory: "DSP_PROG",
stackMemory: "DSP_PROG",
l1DMode: "32k",
l1PMode: "32k",
l2Mode: "32k"
};
...
Dsp.cfg:
...
/* shared region configuration */
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
/* configure SharedRegion #0 (IPC) */
var SR0Mem = Program.cpu.memoryMap["SR_0"];
SharedRegion.setEntryMeta(0,
new SharedRegion.Entry({
name: "SR0",
base: SR0Mem.base,
len: SR0Mem.len,
ownerProcId: MultiProc.getIdMeta("HOST"),
cacheEnable: false,
isValid: true
})
);
/* configure SharedRegion #1 (MessageQ Buffers) */
var SR1Mem = Program.cpu.memoryMap["SR_1"];
SharedRegion.setEntryMeta(1,
new SharedRegion.Entry({
name: "MessageQ Buffers",
base: SR1Mem.base,
len: SR1Mem.len,
ownerProcId: MultiProc.getIdMeta("HOST"),
cacheEnable: false,
isValid: true
})
);
....
Host-Application:
void Application_Start(void)
{
Register_Notify_Callback(LOGGER_NOTIFY_EVENTID, Log_Callback);
printf("Hello from Application.\n");
int dspId = MultiProc_getId("DSP");
// reader does: MessageQ_create(), MessageQ_get(), MessageQ_free() and MessageQ_delete()
HeapBufMP_Params heapParams;
MessageQ_Params msgqParams;
// create heap for messages
HeapBufMP_Params_init(&heapParams);
heapParams.name = "Heap:1";
heapParams.regionId = 1; // SR id
heapParams.blockSize = 64;
heapParams.numBlocks = 10;
HeapBufMP_Handle heapHandle = HeapBufMP_create(&heapParams);
if (heapHandle == NULL)
{
printf("Failed to create a HeapBufMP\n");
return;
}
// register heap with MessageQ
int status = MessageQ_registerHeap((Ptr)(heapHandle), 1);
if (status < 0)
{
printf("Failed to register HeapBufMP with MessageQ\n");
return;
}
MessageQ_Params_init(&msgqParams);
MessageQ_Handle msqHandle = MessageQ_create("MSQ:1", &msgqParams);
printf("Sending request\n");
Request_Data_Stream(dspId);
printf("Waiting for msg on MSQ:1.\n");
Data_Msg *msg;
MessageQ_get(msqHandle, (MessageQ_Msg *)&msg, 2000);
//printf("Got msg with data: %d", msg->data);
//MessageQ_free((MessageQ_Msg)msg);
MessageQ_delete(&msqHandle);
MessageQ_unregisterHeap(1);
HeapBufMP_delete(&heapHandle);
printf("Application finished.\n");
}
DSP-Application:
void Application_Start(void)
{
int hostId = MultiProc_getId("HOST");
Register_Notify_Callback(DATA_REQUEST_NOTIFY_EVENTID, Data_Request_Callback);
notifySem = Semaphore_create(Semaphore_Mode_COUNTING, NULL, NULL);
Semaphore_pend(notifySem, BIOS_WAIT_FOREVER);
// writer does MessageQ_open(), MessageQ_alloc(), MessageQ_put() and MessageQ_close()
MessageQ_QueueId msqId;
Log_Print("star");
// Open msgq
while (MessageQ_open("MSQ:1", &msqId) < 0);
Log_Print("open");
// alloc
Data_Msg *msg = (Data_Msg*) MessageQ_alloc(1, sizeof(Data_Msg));
Log_Print("allo");
msg->data = 123;
// send
/*if(MessageQ_put(msqId, (MessageQ_Msg)msg)<0)
{
Log_Print("ohhh");
MessageQ_close(&msqId); Semaphore_delete(¬ifySem);
return;
}
Log_Print("sent");*/
// close
MessageQ_close(&msqId);
Log_Print("done");
Semaphore_delete(¬ifySem);
}
The console output is:
+ ./slaveloader startup DSP server_dsp.xe674
Attached to slave procId 0.
Loading procId 0.
Loaded file server_dsp.xe674 on slave procId 0.
Started slave procId 0.
+ ./app_host
Hello from Application.
Sending request
DSP-Logger: star
DSP-Logger: open
DSP-Logger: allo
DSP-Logger: done
Waiting for msg on MSQ:1.
Application finished.
Assertion at Line no: 380 in /home/omap/AragoProject/syslinkBios/syslink_2_21_01_05/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/utils/hlos/knl/ResTrack.c: (elem == NULL) : failed
+ ./slaveloader shutdown DSP
Stopped slave procId 0.
Unloaded slave procId 0.
Detached from slave procId 0.
But when I uncomment the sending part in the DSP application:
// send
if(MessageQ_put(msqId, (MessageQ_Msg)msg)<0)
{
Log_Print("ohhh");
MessageQ_close(&msqId); Semaphore_delete(¬ifySem);
return;
}
Log_Print("sent");
I get:
Hello from Application.
Sending requestAssertion at Line no: 1194 in /home/omap/AragoProject/syslinkBios/syslink_2_21_01_05/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/ListMP.c: (localHeadNext != NULL) : failed
DSP-Logger: star
DSP-Logger: open
Assertion at Line no: 1200 in /home/omap/AragoProject/syslinkBios/syslink_2_21_01_05/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/ListMP.c: (elem != NULL) : failed
Assertion at Line no: 1601 in /home/omap/AragoProject/syslinkBios/syslink_2_21_01_05/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/SharedRegion.c: (id < SharedRegion_module->cfg.numEntries) : failed
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = c0004000
[00000000] *pgd=00000000
Internal error: Oops: 17 [#2] PREEMPT
last sysfs file: /sys/devices/platform/davinci_mmc.0/mmc_host/mmc0/mmc0:0002/block/mmcblk0/dev
Modules linked in: syslink ipv6 minix
CPU: 0 Tainted: G D (2.6.37+ #3)
PC is at ListMP_getHead+0x1a8/0x2c8 [syslink]
LR is at SharedRegion_isCacheEnabled+0x148/0x190 [syslink]
pc : [<bf08eff0>] lr : [<bf082d04>] psr: 60000013
sp : c7b65ee8 ip : 00000000 fp : c7b65f14
r10: 00000000 r9 : 00000000 r8 : 00000000
r7 : c9ec1900 r6 : 00000000 r5 : c9f31000 r4 : 00000000
r3 : 00000000 r2 : 00000000 r1 : 00060000 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 0005317f Table: c7aec000 DAC: 00000017
Process kernelThread_6 (pid: 598, stack limit = 0xc7b64270)
Stack: (0xc7b65ee8 to 0xc7b66000)
5ee0: 00000000 6e65706f 6e65706f bf13e224 c9f2e000 00000000
5f00: c9ec1900 00000002 c7b65f3c c7b65f18 bf0a8984 bf08ee58 00000000 00000002
5f20: c9f2e000 00000000 c9ef6000 00000002 c7b65f64 c7b65f40 bf085fb0 bf0a88e8
5f40: 00000000 00000000 c7b65f6c c9eed000 c9ec1800 00000100 c7b65f94 c7b65f68
5f60: bf0a4ac4 bf085efc 00000001 c9ef3000 c9ef3018 c9ef3014 c9ef301c c9ef3020
5f80: 00000000 00000000 c7b65fbc c7b65f98 bf07ff74 bf0a49e4 c7b65fcc c5cdbc38
5fa0: c9ef3000 bf07feec 00000000 00000000 c7b65ff4 c7b65fc0 c005ed74 bf07fefc
5fc0: c5cdbc38 00000000 c9ef3000 00000000 c7b65fd0 c7b65fd0 c5cdbc38 c005ece8
5fe0: c0048220 00000013 00000000 c7b65ff8 c0048220 c005ecf8 00000000 00000000
Backtrace:
[<bf08ee48>] (ListMP_getHead+0x0/0x2c8 [syslink]) from [<bf0a8984>] (_TransportShm_notifyFxn+0xac/0x100 [syslink])
r8:00000002 r7:c9ec1900 r6:00000000 r5:c9f2e000 r4:bf13e224
[<bf0a88d8>] (_TransportShm_notifyFxn+0x0/0x100 [syslink]) from [<bf085fb0>] (Notify_exec+0xc4/0x110 [syslink])
r5:00000002 r4:c9ef6000
[<bf085eec>] (Notify_exec+0x0/0x110 [syslink]) from [<bf0a4ac4>] (_NotifyDriverShm_ISR+0xf0/0x144 [syslink])
r6:00000100 r5:c9ec1800 r4:c9eed000
[<bf0a49d4>] (_NotifyDriverShm_ISR+0x0/0x144 [syslink]) from [<bf07ff74>] (Thread_callback+0x88/0xf8 [syslink])
[<bf07feec>] (Thread_callback+0x0/0xf8 [syslink]) from [<c005ed74>] (kthread+0x8c/0x94)
r9:00000000 r8:00000000 r7:bf07feec r6:c9ef3000 r5:c5cdbc38
r4:c7b65fcc
[<c005ece8>] (kthread+0x0/0x94) from [<c0048220>] (do_exit+0x0/0x6e0)
r7:00000013 r6:c0048220 r5:c005ece8 r4:c5cdbc38
Code: e3a01008 e59f2108 e3a03001 ebff800d (e5940000)
Waiting for msg on MSQ:1.
---[ end trace b3f7d1b6dd6a3d89 ]---
I can't figure out what I'm doing wrong. Any hints?