Other Parts Discussed in Thread: SYSBIOS
Hi,
Looking at configuro documentation (I am using xdctools_3_23_03_53), there is a note about compiler.opt
*********
outdir/compiler.opt
A file containing C compiler command-line flags. These flags must included on the compiler command line for any C source file that directly accesses the RTSC content. The flags define the header file include paths, and machine-mode compiler flags to ensure object code compatibility between all included content.
***********
My question is about which files need to use this. It says that all RTSC content should use this. Does this mean code which uses packages like xdc/runtime or sysbios should use these flags.
I have a few libraries in our system which use these packages. For example, I have a little profiling module which uses xdc/runtime/Timestamp. I am not using CCS to put together and build our projects. Just old fashioned editor and make is how the libraries are built. When these libraries are built, there is no config file and linker.cmd getting generated and things like that.
So, is it important that compiler.opt generated flags be included for building these libraries as well or if I include the correct packages, I should be good to go.
I am hoping that it is fine to just have manual definition of compile flags as long as I am pointing at the right packages.
I do see compiler.opt generate things like
-Dxdc_target_types__="ti/targets/elf/std.h" -Dxdc_target_name__=C674 -Dxdc_cfg__header__=
I am not sure how or where these are used. Other than these, I see standard flags.
Cheers,
-raja.