This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C interrupts on C5509A using C5509_CSL



Hello: I am trying to get the example code from C55xxCSL\examples\generic5509\csl\i2c\i2c1\main_i2c1.c  to generate interrupts for any of the plugged events i.e.

        myALIsr,
        myNACKIsr,
        myARDYIsr,
        myRRDYIsr,
        myXRDYIsr
as shown in  C55xxCSL\examples\generic5509\csl\i2c\i2c1\myIsrs_i2c1.c

I do not ever see any interrupts i.e the  printf(s) in myIsrs_i2c1.c 

I am running on Spectrum Digital C5509A DSK using CCS 5.3. the .cmd is also shown below.

Basically this is off the shelf unmodified code and project from the C55xxCSL library.

Can anyone help and tell me why no interrupts ?

Thanks

Brian

-----------------------------------------------------------------------------------------------------

myIsrs_i2c1.c

/*
 * Copyright (C) 2003 Texas Instruments Incorporated
 * All Rights Reserved
 */
/*
 *---------myIsrs_i2c1.c---------
 * Function definitions for ISR/callBack functions
 */
#include <stdio.h>    
#pragma CODE_SECTION (myALIsr,"myisrSeg");
#pragma CODE_SECTION (myNACKIsr,"myisrSeg");
#pragma CODE_SECTION (myARDYIsr,"myisrSeg");
#pragma CODE_SECTION (myRRDYIsr,"myisrSeg");

void myALIsr()
{
   printf("I2C Arbitration Interrupt Occurred\n");
   asm("\tNOP                       ;====> I2C periodic interrupt routine");   
 
}   

void myNACKIsr()
{
   printf("I2C  NACK Interrupt Occurred\n");
   asm("\tNOP                       ;====> I2C periodic interrupt routine");   
 
}

void myARDYIsr()
{
   printf("I2C ARDY Interrupt Occurred\n");
   asm("\tNOP                       ;====> I2C periodic interrupt routine");   
 
}

void myRRDYIsr()
{
   printf("I2C RRDY Interrupt Occurred\n");
   asm("\tNOP                       ;====> I2C periodic interrupt routine");   
 
}

void myXRDYIsr()
{
   printf("I2C XRDY Interrupt Occurred\n");
   asm("\tNOP                       ;====> I2C periodic interrupt routine");   
 
}

main_i2c1.c /*
 * Copyright (C) 2003 Texas Instruments Incorporated
 * All Rights Reserved
 */
/*
 *---------main_i2c1.c---------
 * This example is desinged to show how to use the I2C   
 * module's interrupt dispatch function. Because there   
 * are several possible events that could trigger a HW   
 * interrupt to the CPU for I2C, a dispatcher was written
 * to enable read of the I2C status to determine which   
 * event/s triggered the HW interrupt and to call a User
 * defined function to service any masked I2C event that
 * needs acknowledgement. This example shows how to build
 * an ISR call back table for use with the I2C dispatcher
 */
#include <csl.h>
#include <csl_i2c.h>
#include <stdio.h>
#include "myIsrs_i2c1.h"

//---------Global data definition---------
Uint16 mask = 1;    
Uint16 enable = 1;    
Uint16 databyte1[2]={0xA,0xB};  
int i=0,x;         

/* Declare and Initialize an I2C call Back Structure */
I2C_IsrAddr addr = {  
        myALIsr,
        myNACKIsr,
        myARDYIsr,
        myRRDYIsr,
        myXRDYIsr
};       

/* Declare and Initialize an I2C initialization structure */
I2C_Setup Init = {

        0,              /* 7 bit address mode */
        0x0020,         /* own address - don't care if master */
        144,            /* clkout value (Mhz)  */
        400,            /* a number between 10 and 400*/
        0,              /* number of bits/byte to be received or transmitted (8)*/
        0,              /* DLB mode on*/
        1               /* FREE mode of operation on*/

};

//---------Function prototypes---------

/* Reference start of interrupt vector table       */
/* This symbol is defined in the file, vectors.s55 */
extern void VECSTART(void);

#pragma CODE_SECTION (taskFunc, "tskSeg");
void taskFunc(void);

//---------main routine---------
void main(void)
{
    // Initialize CSL library - This is REQUIRED !!!
    CSL_init();
/*
    // Set IVPD/IVPH to start of interrupt vector table
    IRQ_setVecs((Uint32)(&VECSTART));
    
    // Call I2C example task/function
    taskFunc();
*/
}

void taskFunc(void) {

    /* Initialize the I2C using the iniitalization structure values */
    I2C_setup(&Init);

    /* Set call back functions for I2C interrupt events */
    I2C_setCallback(&addr);             // hook up the interrupt functions
    
    /* Enable RRDY interrupt */
    I2C_eventEnable(I2C_EVT_RRDY);  
 
    /* Enable all maskable interrupts */
    IRQ_globalEnable();                 // Enable interrupts
    
    /* Write a data byte to I2C */
    x=I2C_write(databyte1,1,1,0x20,1,30000);
   
    if(!x) printf ("\nTEST PASSED\n");
    else printf ("\nTEST FAILED\n");
      
   /* Give some time for interrupt to occur */                                                                   
   for(i=0;i<10000;i++){
   };   
}