Other Parts Discussed in Thread: AM3358
Team,
I'm walking through Sitara Linux Training: uboot debug and i'm hitting a couple of issues.
1 - Perform SPL Debug: I cannot set HW breakpoint at line 582. I set them and there is an exclamation point saying 'evm.c, line 582 [S/W BP disabled]. It says there is no code associated w/ the evm.c file compared to loaded symbols.
i can single step but no breakpoint.
i did rebuild u-boot and spl per instructions
2 - evm.c is not located in /u-boot-xx.xx.xx/board/ti/am335x. I did find it in /ti-sdk-am335x-evm-05.06.00.00/board-support/board-port-labs/sitara-board-port-uboot/board/ti/am335x though.
3 - Is there a need to use the AM3358 EVM GEL file when running this lab?
Thanks.
Marc