Other Parts Discussed in Thread: TMS320C6672
Hi, I am using tms320c6672 with one ddr3 memory(1333MHz, 256MB).
I saw the PHY Calc and Register Calc spread sheet.
1. Should I use PHY Calc spreadsheet for configuring DDR3 memory?
2. In Register Calc spreadsheet, SD_TIM1, SD_TIM2, SD_TIM3, SDCFG, SDRFC register can be calulated. Are these things sufficient for DDR3 configuration?
3. Is it possible to use 1333MHz DDR3 memory with DSP PLL if I use 25Mhz input to DDRCLK? or should I consider the noise problem?
Any answer will be gratefull for me.
Best regards,
Choi Su Young