hai i has gone through the dma controller in the ezdsp5505 and when i transfer the data from the source to the destionation buffer it works with the chip support library and i was little bit confused how to use the dma controller for ping pong buffer if the data length is 1024 .