This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About how to read sensor register in ducati 2.2 code

Hi,Omap experts.

I'm using blaze board, it's omap 4470, and ducati version is 2.2.

i want to use AEC&AGC of OV5650 sensor, so i changed in configscript27fps

 { WRITE, { 0x35030001, 0x00 } },  //0x03

and i stopped what is done in ov5650_setExpGain(I found that if i completely comment out all sensor writing operation,

camera will stop working at the first beginning, so i add a counter so that after ov5650_setExpGain is called 900times, function will be

returned without doing anything )

i found after a while, mms2 AE will stop working because ov5650_setExpGain is doing nothing.

but it seems that AEC&AGC is not starting to work.

I tried to use GetDataFromSensor to read sensor registers value but camera hang when this function is called.

can you help me out on How could i read Sensor registers in OV5650 sensor driver code.

Thanks!

Best regards,

Christian.