Is there a way to get the Davinci auto exposure (AEW) based only on information from a small region of interest of the image (ROI) instead of the whole image (the ROI size is the haff of the original one and located in the image center) ?
This will allow me to get correct exposure in the center of images containing initially dark zones or dark hole areas, even if the surrounding is overexposed).
I have looked on the VPFE documentation (sprue38) specially on the H3A section, but did not find whether it is really possible.
I am using the Linux 2.6.32 with dvdsk 2.00.00.22 and DM6446 DSP.
I would appreciate any help on this point !