This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI_instance 0 Problem

Hello everybody.

I have an issue I can’t understand.

First I’m using the following tools & software:

Omapl 138 EVM board – Code Composer V5.3 – Psp bios V3.00.01 Cslr SPI Example

Using J13 to monitor SPI0 signals (SPI0_Clk, SPI0_SOMI and SPI0_SIMO) on oscilloscope.

I can run the Cslr SPI example without any problems and I can see what I send (as example configures SPI0 in Loopback mode)

1-      The problem is that the SPI0 Clock is always as shown (when power the board up , before and after transmit data from SPIDAT1) in Pic (Even if disabling Loopback mode)

Where  D0 => SPI0_Clk

                D1 => SPI0_SOMI

                D2 => SPI0_SIMO

 

 

2-      When I tried to use SPI0 in normal mode (Loopback mode disabled) the same issue still exists

Is there something is missing in the configuration of SPI 0 instance?

 

Note:

I have already tried the same example with SPI1 with having no problems (SPI1_Clk, SOMI and SIMO works fine).

SPI project is attached with Loopback mode disabled for SPI0. 

SPI_Cslr.rar