Hi
Our custom board has 2 C6678 dsp ( DSP1-- C6678 silicon version 1.0 & DSP2 -- C6678 silicon version 2.0) on the same board.
Both Dsp's are connected to SRIO Switch.
DSP1 of silicon version 1.0 got trained with switch ( port ok , NO Input output error stopped state)...able to transfer srio data thru switch
DSP2 of silicon version 2.0 has issue.
SRIO Loopback is working in DSP2.
But when enabled Normal Operation in DSP2 after training with switch shows Port Ok but Input and output error stopped state is set.
Code used is DIOISR . Its working for DSP1 but DSP2 shows above issue.
We have used Same SRIO Clock source for DSP1 & DSP2..
Please suggest