This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fixed-Point FFTs using C64x+ DSP Library



Hello,

We are looking at using several of the FFTs and IFFTs that are included in the TMS320C64x+ Little-Endian DSP Library.  Can TI supply either C code or Matlab functions that are equivalent fixed-point implementations?

I have seen other posts refer to the examples for the FFTs that include C functions, but the install that I have does not include the code for these examples - the folders are empty.  I downloaded the latest version -  dsplib_c64Px_3_1_1_1_Win32, and this did not have examples either for the FFTs.

Do these examples have the FFTs fully implemented in fixed-point C?  If yes, where are they located?

Thank you for help.

Regards,

Dan