Other Parts Discussed in Thread: OMAP-L138
Hello,
I have just started to use ZOOM OMAP-LI138 EVM with OMAP-L138 SOM-M1. I want to use the C6748 processor of the SOM with CCS V 4.2.4. For startup i have gone through the document " 1020208B_AN492_Using_CCSv4-2-4_with_SOM-M1", but i am facing following problems:
1) Section 2.1 of document says that to replace "desc" with "description". I opened the file c6748 in notepad and replaced all desc with description but when i tried to save it, it says file is read only. How to approach this problem.
2)Is blackhawk emulator is also required to be connected for ZOOM OMAP-LI138 EVM with OMAP-L138 SOM-M1/C6748 SOM-M1.
3) I followed the complete steps in the document except section 2.1 but in the end when i connected board with USB cable to PC, and pressed debug button, it gave error message that target configured is not done properly. Can you send me the steps for target configuration that works. I will also appreciate if you can send me any video/document for CCS V4.2.4.
Thanks,
Sinha