This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3730 processor module Rev G with OMAP3530 EVM Rev D + 4bit ECC NAND

Other Parts Discussed in Thread: OMAP3530, DM3730
Is it possible to use OMAP3730 processor module Rev G with Mistral OMAP3530 EVM Rev D?
 
I need to Migrate to OMAP3730 SoM RevD  + OMAP3 EVM RevG (Use 4 bit ecc)
 
Is it sufficient to apply Patch for 4/8 bit ECC on PSP 3.00.01.06(Kernel 2.6.32)? Still after applying the patch, I find these errors occurring continuously:- "mtd->read()" and "returned ECC error".

What additional changes I need to do? Can anyone help?