This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ipcInM3Link error

Hi,

Some errors occur in ipcInM3Link like this:

[m3video]  256230: Assertion @ Line: 101 in links_common/ipcInM3/ipcInM3Link_tsk.c: pObj->prd.clkHandle != NULL : failed !!!

What causes it?

 

  • Clock create can fail either due to memory allocation failure or due to wrong clock configuration. Have you made any changes to /ipcInM3Link_tsk.c ? If not pls share the full log and usecase file for analysis.

  • call the VcapVenc_start() function

    /*******************************************************************************
     *                                                                             *
     * Copyright (c) 2011 Texas Instruments Incorporated - http://www.ti.com/      *
     *                        ALL RIGHTS RESERVED                                  *
     *                                                                             *
     ******************************************************************************/
    /**
      \file my_vcap_venc.c
      \brief
      */
    #include "mcfw/src_linux/mcfw_api/usecases/multich_common.h"
    #include <my_vcap_venc.h>
    
    
    VcapVenc_Ctrl gVcapVenc_ctrl;
    
    
    
    Void myVsysInit(Bool hdDemo)
    {
    	VSYS_PARAMS_S vsysParams;
    
    	UInt32 useCase;
    
    
    	Vsys_params_init(&vsysParams);
    	if(hdDemo)
    		useCase = VSYS_USECASE_MULTICHN_HD_VCAP_VENC;
    	else
    		useCase = VSYS_USECASE_MULTICHN_VCAP_VENC;
    
    
    	vsysParams.systemUseCase        = useCase;
    	vsysParams.enableCapture        = TRUE;
    	vsysParams.enableNsf            = TRUE;//FALSE;
    	vsysParams.enableEncode         = TRUE;
    	vsysParams.enableDecode         = FALSE;
    	vsysParams.enableNullSrc        = FALSE;
    	vsysParams.numDeis              = 2;
    	if(hdDemo)
    	{
    		vsysParams.numSwMs              = 0;
    		vsysParams.numDisplays          = 2;
    		vsysParams.enableSecondaryOut   = FALSE;//TRUE;
    		vsysParams.enableMjpegEnc       = FALSE;//TRUE;
    		vsysParams.enableSclr           = FALSE;//TRUE;
    		vsysParams.enableOsd            = FALSE;//TRUE;
    		vsysParams.enableScd            = FALSE;//TRUE;
    	}
    	else
    	{
    		vsysParams.numSwMs              = 1;
    		vsysParams.numDisplays          = 1;
    		vsysParams.enableSecondaryOut   = TRUE; /* NOT USED for this use case */
    		vsysParams.enableMjpegEnc       = TRUE;
    		vsysParams.enableOsd            = TRUE;
    		vsysParams.enableScd            = TRUE;
    	}
    	if (vsysParams.enableSecondaryOut)
    	{
    		if(vsysParams.enableMjpegEnc == FALSE)
    			gDemo_info.maxVencChannels *= 2;
    		else
    			gDemo_info.maxVencChannels *= 3;
    	}
    
    	if(hdDemo)
    	{
    		gDemo_info.maxVcapChannels = 2;
    		gDemo_info.maxVdisChannels = 0;
    		gDemo_info.maxVencChannels = 2;//4;
    		gDemo_info.maxVdecChannels = 0;
    	}
    	else
    	{
    		gDemo_info.maxVcapChannels = 16;
    		gDemo_info.maxVdisChannels = 16;
    		gDemo_info.maxVencChannels = 16;
    		gDemo_info.maxVdecChannels = 0;
    	}
    
    	Vsys_init(&vsysParams);
    
    }
    
    Void MyVsysStart(Bool hdDemo)
    {
    	MyVsysInit(hdDemo);
    
    	MyVsysLinkCreate();
    
    }
    
    Void MyVcapStart(Bool hdDemo)
    {
    	MyVcapChnInit(hdDemo);
    
    	MyVcapLinkCreate();
    
        Vcap_start();
    
    }
    
    Void MyVencStart(Bool hdDemo)
    {
    	MyVencChnInit(hdDemo);
    
    	/* Init the application specific module which will handle bitstream exchange */
    	VcapVenc_bitsWriteCreate();
    
    	MyVencLinkCreate();
    
    	Venc_start();
    
    }
    
    Void VcapVenc_start(Bool hdDemo)
    {
    
    	MyVsysStart(hdDemo);
    
    	MyVcapStart(hdDemo);
    
    	MyVencStart(hdDemo);
    
    }
    
    Void VcapVenc_stop()
    {
        VSYS_PARAMS_S contextInf;
        Vsys_getContext(&contextInf);
    
        /* Stop components */
        Vcap_stop();
        Venc_stop();
    
        VcapVenc_bitsWriteDelete();
    
        Vsys_delete();
    
        /* De-initialize components */
        Vcap_exit();
        Venc_exit();
        Vsys_exit();
    }
    
    

    1401.log.rtf

  • The issue is because the ipcInM3 link is not created but you are starting the link. The file you shared is not a usecase file. I don't see Vsys_create being done . Pls check you usecase file and ensure links that you don't use have linkID set to INVALID ID.

  • Thanks, Badri. The ipcInM3 link issue has been settled, but another problem arised. I found it does not signal the gVcapVenc_ctrl.wrSem semophore, so it stop here:

    status = OSA_semWait(&gVcapVenc_ctrl.wrSem, OSA_TIMEOUT_FOREVER);

    And this issue due to no newDataAvailable for encode:

    callback.newDataAvailableCb = VcapVenc_bitsWriteCbFxn;

    Why the encoder fail to get new data?

  • Pls check your usecase file where the link connections are setup to ensure you are connecting them correctly and you are starting all links.Also check the logs of Vsys_printBufferStatistics to see in which links buffers are getting locked.

  • Hi, Badri. The usecase can work normally now. I've changed ipcOutVpssPrm.notifyNextLink from TRUE to FALSE and ipcOutVpssPrm.noNotifyMode from FALSE to TRUE. And it seems no need to start ipcM3In Link.

     ipcOutVpssPrm.notifyNextLink            = FALSE;//TRUE;//FALSE;
     ipcOutVpssPrm.notifyPrevLink            = TRUE;
     ipcOutVpssPrm.noNotifyMode              = TRUE;//FALSE;