This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sine wave TMS320C5416 assembly language program "output section" warnings



hi

i am getting another warnings while compiling for sine wave TMS320C5416 processor in assembly language. i use to get these in many programs.what they say and how to remove them?

these are the warnings i got:
<Linking>
>> warning: creating output section COSINE without SECTIONS specification
>> warning: creating output section STACK without SECTIONS specification
>> warning: creating output section CODE without SECTIONS specification
>> warning: entry point symbol _c_int00 undefined

Build Complete,
  0 Errors, 4 Warnings, 0 Remarks.

and here's the code for sine wave i tried:

FREQ1000 .set 1486
FREQ1750 .set 2600
FREQ2000 .set 2972
FREQ3000 .set 4458
FRAME_SIZE .set 64
    .mmregs
    .include "cos256_tbl.inc"
    .global COSINE_BUFFER
    .global FREQ_BUFFER
    .bss TEMP,1
    .bss FREQ_BUFFER,128
    .bss COSINE_BUFFER,257
    .bss _FREQ_STEP,1
    .bss _INIT_PHASE,1
    .def FREQ
STK .usect "STACK",100
    .mmregs
    .sect "CODE"
FREQ:
    SSBX OVM
    SSBX SXM
    SSBX FRCT
    NOP
    NOP
    STM #STK+100H,SP
    STM #001EH,PMST
    ST #FREQ1000,*(_FREQ_STEP) ;
    ST #0,*(_INIT_PHASE) ;
    STM #FREQ_BUFFER,AR3 ;
    CALL COPY_COS_TBL ;
    CALL GEN_FREQ ;
LOOP:
    B LOOP ;

GEN_FREQ:
    STM #FRAME_SIZE-1,BRC ;
    RPTB sine1-1
    LD *(_FREQ_STEP),A ;
    ADD *(_INIT_PHASE),A ;A=PRESENT PHASE
    STL A,*(_INIT_PHASE) ;SAVE PRESENT PHASE
    SUB #4000H,A ;SUB PI/2 FOR SINE
    ABS A ;Acc CONTAINS THE OFFSET
    STL A,*(TEMP) ;
    LD *(TEMP),9,A ;
    STH A,*(TEMP) ;
    LD *(TEMP),A ;
    ABS A ;
    ADD #COSINE_BUFFER,A ;
    STLM A,AR2 ;
    nop ;
    nop ;
    LD *AR2,A ;
    STL A,*AR3+ ;

sine1:
    NOP ;
    RET ;
COPY_COS_TBL:
    STM #COSINE_BUFFER,AR2
    RPT #257-1
    MVPD #COSOFF,*AR2+
    RET

what's the problem now?