Hello Community,
I've read trough several threads in this forum but no final solution was given so far, so I'm just going to ask the question my way and maybe someone will be able to answer it.
I'm trying to use connector J10 as a 2nd UART but still keep ttyO0 untouched.
As far as i read, it should be possible to use this connector in Profile 2.
The LCD needs to work as well at the same time.
I had a fast look trough the pinmuxing-tools, but since i never used anything like that before,I dont really want to tough it, if possible.
So my question is:
Is it possible to use untouched ttyO0 as console, J10 as UART and LCD at the same time?
If it requires pinmuxing, do i need to compile the kernel again after changing the pinmux-configuration?
regards,
Sebastian