Hi, I am trying to port some legacy code used with CCS3 to CCS5. This code has been written to run on a custom board with a DM6437 chip.
I have installed the following packages:
bios_5.31.08.15
ccs_5.3.0
dvsdk_1_11_00_00
ndk_1_93
pspdrivers_1_10_03
Some of the original source files include cslr_sysctl.h which I cannot locate anywhere inside the installed packages.
The file using this include performs grabs from the vport.
Could you suggest where the cslr_sysctl.h comes from and which packages need to be installed to satisfy the dependency ?
Thanks a lot,
Todor