Hi,
I was reading the EMIF 16 user guide and I have some questions:
1 - How is WE Strobe Mode selected (I didn't find a specific bit for that)? This can be done only for CE3, right?
2 - In section 2.5.5 we have that "The Select Strobe (SS) Mode is selected when the 'ss' bit in Async Wait Cycle Config Register (AWCCR) is set to '1'. SS mode overrides the WE strobe mode when 'ss' = 1." The 'ss' bit actually is part of ASYNC registers, right?
3 - According to section 2.4 we have two operation modes for EMIF16 (WE Strobe and Select Strobe). Section 2.5.4 is about waveforms, my question is: how the waveforms of 2.5.4.1 (Asynchronous Reads) and 2.5.4.2 (Asynchronous Writes) are obtained? Is making 'ss' bit zero for CE0-2? This way we would have three different operation modes.
Thanks