OMAPL138 Champs,
I've looked through both the datasheet and the TRM but have been unable to find the internal reistance values of the Pull up and Pull down resistors that are determined by the PUPD_ENA and PUPD_SEL registers. These registers have default states which are listed in 11.5.22 Pullup/Pulldown Enable Register and 11.5.23 Pullup/Pulldown Select Register in the TRM
There is also information on how oppose and compliment the resistors.