Other Parts Discussed in Thread: TMS320C6657
hi sirs,
I try to reduce cycles of memory accessing of TMS320C6657.
I got 56 cycles of accessing uPP configuration memory which I wandered is it cost too much?
If yes, could you teach me how could I reduce cycles?
Part of test code is below.
int t1 = 0;
int t2 = 0;
int diff = 0;
typedef struct
{
unsigned int FREE: 1;
unsigned int SOFT: 1;
unsigned int RTEMU: 1;
unsigned int EN: 1;
unsigned int SWRST: 1;
unsigned int r6_5: 2;
unsigned int DB: 1;
unsigned int r31_8: 24;
} UPPCR_BIT;
main
{
TSCL = 0;
UPPCR_BIT *uppcr = (UPPCR_BIT *)0x02580004;
t1 = TSCL;
// Ensure uPP not enabled yet.
uppcr->EN=0;
t2 = TSCL;
diff = t2-t1;
}
Thank you in advance
bai