This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tvp5150am1 issue AM3517

Other Parts Discussed in Thread: TVP5150AM1, AM3517, TVP5150

Hello Everyone.

 I am having problems with tvp5150am1 video micro and ARM A8 Cortex (Texas Instruments AM3517). I am using linux kernel (2.6.37) with busybox.

 Micro is connected in I2C-2 bus. In my board I setup tvp5150am1 in this way:

 static struct i2c_board_info __initdata i2c2_boardinfo[] = {
 /*Video Input */
 {
 I2C_BOARD_INFO("tvp5150", 0x5c),
 .type ="tvp5150"

 },

 };
 ...
 i2c_register_board_info(2, i2c2_boardinfo, ARRAY_SIZE(dinitel_i2c2_boardinfo));


 And if I do a dmesg I can see this:

 "Linux video capture interface: v2.00
 device class 'video4linux': registering
 bus: 'i2c': add driver tvp5150
 bus: 'i2c': driver_probe_device: matched device 2-005c with driver tvp5150
 bus: 'i2c': really_probe: probing driver tvp5150 with device 2-005c
 tvp5150 2-005c: chip found @ 0xb8 (OMAP I2C adapter)
 driver: '2-005c': driver_bound: bound to device 'tvp5150'
 bus: 'i2c': really_probe: bound device 2-005c to driver tvp5150"

 But I don't have any /dev/videox or /dev/mediax. Any idea what is happening? I checked out the corresponding pins are  (CAM_D0, CAM_D1, CAM_D2... CAM_D7, CAM_HS, CAM_VS, CAM_PCLK, CAM_FLD) in mode 0



 A lot of thanks