Hi OMAP Team,
I am currently following the http://processors.wiki.ti.com/index.php/Building_The_OMAP-L137_SDK in order to re-build all the SDK for my OMAP-L137. There are four builds described in this instructions.
1. Build CMEM
2. Build DSPLink
3. Build Codec Engine Examples
4. Build Codec Server
Is there a documentation defines check points of each building process? I mean a documentation defines which re-built files should be existed at which location so that i can then do the manually checking on these re-built files as my verifications.
For example, during the CMEM building process, the make installation copies some files to some locations. I am looking for a documentation that describes all re-built files in each building step.
Regards,
Ping
Regards,
Ping