This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM on ICE board



I'm trying to get PWM output on an ICE board.

Apology for the long post, there's a lot I'm still learning about ...

From schematic (AM335x_ICE_3h0013_Schematic_Rev 1_0a.pdf)

J12 -> pin41/pin44 = SPI0_D0, SPI0_CLK

Those lines are routed to uC ball A17, B17 that can be re-mux to EHRPWM0A / EHRPWM0B

I am trying to go create a mux for this new configuration.

My baseline application comes from sdk/protocols/ethercat_slave/ecat_appl.

I see that EcatStack/ecat_appl_cnfg.h:

  { 0x0950 , 0 , AM335X_PIN_OUTPUT | AM335X_PIN_INPUT },    //    spi0_sclk
  { 0x0954 , 0 , AM335X_PIN_INPUT },    //    spi0_DO

Using the pin-mux tool, Device Package ZCZ, AM335x Rev1.x, I select the PWM to make it match ball A17, B17

The code generated gives:

MUX_VAL(CONTROL_PADCONF_SPI0_SCLK, (IEN | OFF | MODE3 )) /* ehrpwm0A_mux1 */
MUX_VAL(CONTROL_PADCONF_SPI0_D0, (IEN | OFF | MODE3 )) /* ehrpwm0B_mux1 */

on one hand, I have pin-mux saying

IEN = 1 << 5

OFF = 1 << 3

on the other, I have the sdk saying

/* am335x specific mux bit defines */
#define AM335X_SLEWCTRL_FAST            (0 << 6)
#define AM335X_SLEWCTRL_SLOW            (1 << 6)
#define AM335X_INPUT_EN                 (1 << 5)
#define AM335X_PULL_UP                  (1 << 4)
/* bit 3: 0 - enable, 1 - disable for pull enable */
#define AM335X_PULL_DISA                (1 << 3)
#define AM335X_PIN_OUTPUT               (0)
#define AM335X_PIN_OUTPUT_PULLUP        (AM335X_PULL_UP)
#define AM335X_PIN_INPUT                (AM335X_INPUT_EN | AM335X_PULL_DISA)
#define AM335X_PIN_INPUT_PULLUP         (AM335X_INPUT_EN | AM335X_PULL_UP)
#define AM335X_PIN_INPUT_PULLDOWN       (AM335X_INPUT_EN)

so pin-mux is telling to use (1<<5)|(1<<3), which I read as (AM335X_INPUT_EN | AM335X_PULL_DISA), that is AM335X_PIN_INPUT

I update EcatStack/ecat_appl_cnfg.h with

    { 0x0950 , 3 ,  AM335X_PIN_INPUT },    //    spi0_sclk   // XXX gpio0[2] -> EHRPWM0A             // A17
    { 0x0954 , 3 ,  AM335X_PIN_INPUT },    //    spi0_DO     // XXX gpio0[3] -> EHRPWM0B            // B17
 

My questions are:

1 - whatever I'm doing must be flawed because it does not work. Am I missing some steps?

2- I dont understand pin-mux setting, because I would have expected the value for EHRPWM0A/B somewhat to be an output .. not an AM335X_PIN_INPUT