Hi OMAP Team,
My OMAP-L137 EVM runs MontaVista Linux based SDK and it comes with U-Boot 1.3.3. I am updating to U-Boot-03.20.00.14, which is contained in DaVinci-PSP-SDK-03.20.00.14 package. Could you please provide me the make instruction? It looks like this new U-Boot 03.20.00.14 is based on DaVinci GIT instead of MontaVista. For example, the <>\u-boot-1.3.3\include\config\da8xx_evm.h file no longer exists in the u-boot-03.20.00.14\include\config folder.
Regards,
Ping