This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C55XCSL-LOWPOWER-3.01 Not working - Projects missing .out

7446.CSL_Latest_Release_Notes.pdf

Hello all - 

I am trying to run the example project programs that come with the CSL for the 5515 downloadable here :
http://software-dl.ti.com/dsps/dsps_public_sw/dsps_swops_houston/C55X/latest/index_FDS.html

I am using the TMS320 EzDSP C5535


I am trying to get an example program working by following the C55XCSL-Lowpower-3.01 release notes from December 20, 2012 (see attached). 
I am running CCS v4.2.4.00033 . 

My problem is that:
When i import the projects, and I select any one of them and try to build them, I get the following error:
Errors exist in project "xxxx" (for example "CSL_SPI_Example_Out") 
I click continue however, and I get the error:
"Error occurred during launch
Program File does not exist."

I think its complaining that there is no .out file, which is true, there isnt. 
However I have followed the steps for the 2012 release notes exactly as they are printed, so this should be working. Does anyone know how I can resolve these errors?

All help is appreciated greatly - Im a student in college, very new to microprocessors, code composer suite, and to DSPs entirely.

Nate