Other Parts Discussed in Thread: AM1705
Hi Everybody!
I'm using linux kernel 3.2.2 on Sitara AM1705.
My application has a select() function that checks UART ( /dev/ttyS1 ) for received data. I read incoming data without errors within read(). Then the program redirects received symbols to the main console ( /dev/ttyS0 ).
The problem is in receive data loss on ttyS1. I see this when check received symbols in application buffer.
By the inspection and changing kernel code I found out that RX FIFO trigger (FIFO Control buffer) is set to 8 bytes. So, I tried to change trigger to 1 byte and it makes less data loss. Hence it appears that application can't read out received symbols from UART RX buffer in time! Application consumes max 2.3% of the CPU time (top statistics). Why this is happening?
Has anybody ever encountered this issue? What should I do? Should I change kernel driver or my application?
See my code clippings below =>
....
/* Open second uart with fd */
fd = open("/dev/ttyS1", O_RDWR | O_ASYNC | O_NDELAY);
if (fd == -1) {
/* Could not open the second uart */
SYS_LOG_ERR("unable to open /dev/ttyS1");
return CLI_FAILURE;
}
else {
/* Setup open file flags */
fcntl(fd, F_SETFL, 0);
}
.....
/* Read incoming data */
if ((len = read(fd, msg, (sizeof(msg)-1))) < 0)
{
SYS_LOG_ERR("read from second uart failed");
}
else
{
/* Data redirection */
....
}