TVP5158 Ref design mentions its interface with DM6467 video port. But DM3730 does not have a Video Input port, it only has Camera Sensor Interface , is there a way we can interface TVP5158 and DM3730 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Muhammad,
It is possible to connect TVP5158 and DM3730. Look at the specifications of the TVP5158. TVP5158 provides a glueless audio and video interface to TI DaVinci video processors. Video output ports support 8-bit ITU-R BT.656 and 16-bit 4:2:2 YCbCr with embedded synchronization.
In other hand you can use parallel interface of the DM3730 - ITU mode: In this mode, the image-sensor module provides an ITU-R BT 656-compatible data stream. The horizontal and vertical synchronization signals are not provided to the interface. Instead, the data stream embeds start-of-active video (SAV) and end-of-active video (EAV) synchronization code. This mode works in 8- and 10-bit configurations.
You should use 8-bit configuration.
You can find more detailed description of the Camera ISP in the TRM at the link below:
http://www.ti.com/lit/ug/sprugn4r/sprugn4r.pdf
BR
Tsvetolin Shulev