This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NO Video display with the DM816x / C6A816x /AM389x EVM running MCFW on DVRRDK_03.00.00.00

Other Parts Discussed in Thread: TVP5158

hi ,  there are many errors, when i run the MCFW DEMO on the DM816x / C6A816x /AM389x EVM Baseboard + Expansion I/O Daughtercard.  my  steps  is


1)make all DVRRDK
first, i change the type of board in Rules.make

ifeq ($(DVR_RDK_BOARD_TYPE ), )
  DVR_RDK_BOARD_TYPE := DM816X_EVM
endif

then
$ cd <DVR_RDK_BASE>/dvr_rdk
$ make –s sys_all

2) connect the cable. D1 camera connect to J1 and HDMI camera connect to P3 , J8 connect to screen and P6 connect another screen
 

3) run the demo


root@dm816x:/opt/dvr_rdk/ti816x# ls
bin              init.sh          run.sh           unload.sh
demo_ini         kermod           run_gui.sh       validate.sh
env.sh           load.sh          run_link_api.sh
firmware         open_bin         scripts
root@dm816x:/opt/dvr_rdk/ti816x# ./init.sh
*** Bootargs Validated for mem param ***
*** Bootargs Validated for notifyk.vpssm3 params ***
Kernel bootargs validated
numid=1,iface=MIXER,name='PCM Playback Volume'
  ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
  : values=127,127
  | dBscale-min=-63.50dB,step=0.50dB,mute=0
 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf005020
 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040
SysLink version : 2.10.02.17
SysLink module created on Date:Mar 14 2013 Time:23:12:01
Trace enabled
Trace SetFailureReason enabled
 Setting DMM priority for [DUCATI  ] to [0] ( 0x4e000624 = 0x08000000 )
 Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
 Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 )
 Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 )
 
 *** TVP5158 probe : START ***
 
 TI VS EVM : TVP5158 device address : 0x58, 0x5a, 0x5c, 0x5e
 TI DVR    : TVP5158 device address : 0x5c, 0x5d, 0x5e, 0x5f
 
 Device found     : I2C (0xXX): 0x08 = 0x51
                    I2C (0xXX): 0x09 = 0x58
 
 Device NOT found : I2C (0xXX): Read ERROR !!! (reg[0x08], count = 2)
 
 I2C (0x58): Read ERROR !!! (reg[0x08], count = 2)
 I2C (0x5a): Read ERROR !!! (reg[0x08], count = 2)
 I2C (0x5c): 0x08 = 0x00
 I2C (0x5c): 0x09 = 0x00
 I2C (0x5d): 0x08 = 0x00
 I2C (0x5d): 0x09 = 0x00
 I2C (0x5e): Read ERROR !!! (reg[0x08], count = 2)
 I2C (0x5f): Read ERROR !!! (reg[0x08], count = 2)
 why??
 *** TVP5158 probe : END ***
 
/opt/dvr_rdk/ti816x
root@dm816x:/opt/dvr_rdk/ti816x# ./load.sh
Attached to slave procId 2.
Loaded file ../firmware/dvr_rdk_fw_m3vpss.xem3 on slave procId 2.
Started slave procId 2.
After Ipc_loadcallback status [0x00000000]
 [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 250000000, <NEW> - 280000000
 [m3vpss ] notify_attach  rtnVal  0
 [m3vpss ] initProxyServer  rtnVal  0
 [m3vpss ] 
 [m3vpss ]  *** UTILS: CPU KHz = 560000 Khz ***
 [m3vpss ] 
 [m3vpss ]  43: SYSTEM  : System Common Init in progress !!!
 [m3vpss ]  43: SYSTEM: IPC init in progress !!!
 [m3vpss ]  43: SYSTEM: Attaching to [HOST] ...
 [m3vpss ]  1043: SYSTEM: Attaching to [HOST] ...
 [m3vpss ]  1044: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [m3vpss ]  1044: SYSTEM: Attaching to [DSP] ...
After Ipc_startcallback status [0x097d2000]
Attached to slave procId 1.
Loaded file ../firmware/dvr_rdk_fw_m3video.xem3 on slave procId 1.
Started slave procId 1.
After Ipc_loadcallback status [0x00000000]
 [m3video] ***** SYSTEM  : Frequency <ORG> - 250000000, <NEW> - 280000000
 [m3vpss ]  2045: SYSTEM: Attaching to [DSP] ...
 [m3video] 
 [m3video]  *** UTILS: CPU KHz = 560000 Khz ***
 [m3video] 
 [m3video]  1424: SYSTEM  : System Common Init in progress !!!
 [m3video]  1424: SYSTEM: IPC init in progress !!!
 [m3video]  1424: SYSTEM: Attaching to [HOST] ...
 [m3video]  2423: SYSTEM: Attaching to [HOST] ...
 [m3video]  2425: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [m3video]  2425: SYSTEM: Attaching to [DSP] ...
After Ipc_startcallback status [0x00000000]
Attached to slave procId 0.
Loaded file ../firmware/dvr_rdk_fw_c6xdsp.xe674 on slave procId 0.
Started slave procId 0.
After Ipc_loadcallback status [0x00000000]
 [c6xdsp ] ***** SYSTEM  : Frequency <ORG> - 800000000, <NEW> - 800000000
 [m3video]  3425: SYSTEM: Attaching to [DSP] ...
 [m3vpss ]  3045: SYSTEM: Attaching to [DSP] ...
 [c6xdsp ] 
 [c6xdsp ]  *** UTILS: CPU KHz = 800000 Khz ***
 [c6xdsp ] 
 [c6xdsp ]  5: SYSTEM  : System Common Init in progress !!!
 [c6xdsp ]  5: SYSTEM: IPC init in progress !!!
 [c6xdsp ]  5: SYSTEM: Attaching to [HOST] ...
 [c6xdsp ]  1029: SYSTEM: Attaching to [HOST] ...
 [c6xdsp ]  1031: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [c6xdsp ]  1031: SYSTEM: Attaching to [VIDEO-M3] ...
After Ipc_startcallback status [0x00000000]
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Mar 14 2013 23:18:49
 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf005020
 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040
 [m3vpss ]  4045: SYSTEM: Attaching to [DSP] ...
 [m3video]  4425: SYSTEM: Attaching to [DSP] ...
 [c6xdsp ]  2055: SYSTEM: Attaching to [VIDEO-M3] ...
 [m3vpss ]  5045: SYSTEM: Attaching to [DSP] ...
 [c6xdsp ]  2878: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [m3video]  5425: SYSTEM: Attaching to [DSP] ...
 [c6xdsp ]  2878: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  5425: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [m3video]  5425: SYSTEM: Attaching to [VPSS-M3] ...
 [m3vpss ]  6045: SYSTEM: Attaching to [DSP] ...
 [m3video]  6425: SYSTEM: Attaching to [VPSS-M3] ...
 [c6xdsp ]  3901: SYSTEM: Attaching to [VPSS-M3] ...
 [c6xdsp ]  4524: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [m3vpss ]  7045: SYSTEM: Attaching to [DSP] ...
 [c6xdsp ]  4524: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3vpss ]  7045: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [m3vpss ]  7045: SYSTEM: Attaching to [VIDEO-M3] ...
 [m3video]  7425: SYSTEM: Attaching to [VPSS-M3] ...
 [c6xdsp ]  5547: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3video]  8045: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [m3vpss ]  8045: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  5548: SYSTEM: Creating MsgQ [DSP_MSGQ] ...
 [m3video]  8045: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3vpss ]  8045: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [c6xdsp ]  5548: SYSTEM: Creating MsgQ [DSP_ACK_MSGQ] ...
 [m3video]  8045: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ...
 [m3vpss ]  8045: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3video]  8046: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ...
 [m3vpss ]  8045: SYSTEM: Creating MsgQ [VPSS-M3_MSGQ] ...
 [m3video]  8047: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [m3vpss ]  8045: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ...
 [m3video]  8047: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 [m3vpss ]  8047: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [m3video]  8047: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 [m3vpss ]  8047: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 [m3video]  8047: SYSTEM: IPC init DONE !!!
 [m3vpss ]  8047: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 [c6xdsp ]  5548: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [m3vpss ]  8047: SYSTEM: IPC init DONE !!!
 [c6xdsp ]  5548: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 [m3video]  8053: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB)
 [m3vpss ]  8053: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB)
 [c6xdsp ]  5548: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 [m3video]  8053: MEM: Shared Region 1: Base = 0x90000000, Length = 0x0d000000 (208 MB)
 [m3vpss ]  8053: MEM: Shared Region 1: Base = 0x90000000, Length = 0x0d000000 (208 MB)
 [c6xdsp ]  5548: SYSTEM: IPC init DONE !!!
 [m3video]  8055: SYSTEM  : System Common Init Done !!!
 [m3vpss ]  8055: SYSTEM  : System Common Init Done !!!
 [c6xdsp ]  5550: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB)
 [m3video]  8055: SYSTEM  : System Video Init in progress !!!
 [m3vpss ]  8055: SYSTEM  : System VPSS Init in progress !!!
 [c6xdsp ]  5550: MEM: Shared Region 1: Base = 0x90000000, Length = 0x0d000000 (208 MB)
 [m3video]  8055: SYSTEM  : System Video Init Done !!!
 [m3vpss ] === HDVPSS Clocks are enabled ===
 [c6xdsp ]  5551: SYSTEM  : System Common Init Done !!!
 [m3video]  8056: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
 [m3vpss ] === HDVPSS is fully functional ===
 [c6xdsp ]  5417: SYSTEM  : System DSP Init in progress !!!
 [m3video]  8056: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
 [m3vpss ] === HDVPSS module is not in standby ===
 [c6xdsp ]  5417: SYSTEM  : RpeServer_init() done... Ret Val 0!!!
 [m3video]  8056: SYSTEM: ListElem Shared Addr = 0xbf18b680
 [m3vpss ] === I2C1 Clk is active ===
 [c6xdsp ]  5553: SYSTEM: Creating ListMP [DSP_IPC_OUT_19] in region 0 ...
 [m3video]  8058: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
 [m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_2_0
 [c6xdsp ]  5553: SYSTEM: Creating ListMP [DSP_IPC_IN_19] in region 0 ...
 [m3video]  8058: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
 [m3vpss ]  8060: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
 [c6xdsp ]  5554: SYSTEM: ListElem Shared Addr = 0xbf18eb80
 [m3video]  8058: SYSTEM: ListElem Shared Addr = 0xbf1cdf80
 [m3vpss ]  8060: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
 [c6xdsp ]  5554: SYSTEM: Creating ListMP [DSP_IPC_OUT_20] in region 0 ...
 [m3vpss ]  8061: SYSTEM: ListElem Shared Addr = 0xbf22c480
 [c6xdsp ]  5554: SYSTEM: Creating ListMP [DSP_IPC_IN_20] in region 0 ...
 [m3vpss ]  8063: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
 [c6xdsp ]  5554: SYSTEM: ListElem Shared Addr = 0xbf1aeb00
 [c6xdsp ]  5555: SYSTEM: Creating ListMP [DSP_IPC_OUT_21] in region 0 ...
 [c6xdsp ]  5555: SYSTEM: Creating ListMP [DSP_IPC_IN_21] in region 0 ...
 [c6xdsp ]  5555: SYSTEM: ListElem Shared Addr = 0xbf1d1480
 [m3video]  8064: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_19] in region 0 ...
 [m3vpss ]  8063: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
 [c6xdsp ]  5556: SYSTEM: Creating ListMP [DSP_IPC_OUT_24] in region 0 ...
 [m3video]  8064: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_19] in region 0 ...
 [m3vpss ]  8063: SYSTEM: ListElem Shared Addr = 0xbf22f980
 [c6xdsp ]  5556: SYSTEM: Creating ListMP [DSP_IPC_IN_24] in region 0 ...
 [m3video]  8064: SYSTEM: ListElem Shared Addr = 0xbf232e80
 [m3vpss ]  8076: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_19] in region 0 ...
 [c6xdsp ]  5556: SYSTEM: ListElem Shared Addr = 0xbf1f0e80
 [m3video]  8067: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_20] in region 0 ...
 [m3vpss ]  8077: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_19] in region 0 ...
 [c6xdsp ]  5556: SYSTEM: Creating ListMP [DSP_IPC_OUT_25] in region 0 ...
 [m3video]  8067: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_20] in region 0 ...
 [m3vpss ]  8077: SYSTEM: ListElem Shared Addr = 0xbf291c80
 [c6xdsp ]  5557: SYSTEM: Creating ListMP [DSP_IPC_IN_25] in region 0 ...
 [m3video]  8067: SYSTEM: ListElem Shared Addr = 0xbf252880
 [m3vpss ]  8079: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_20] in region 0 ...
 [c6xdsp ]  5557: SYSTEM: ListElem Shared Addr = 0xbf20ef00
 [m3video]  8070: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_21] in region 0 ...
 [m3vpss ]  8080: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_20] in region 0 ...
 [c6xdsp ] !!WARNING.Resource already registered:2
 [c6xdsp ]  5423: SYSTEM  : Initializing Links !!!
 [m3video]  8070: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_21] in region 0 ...
 [m3vpss ]  8080: SYSTEM: ListElem Shared Addr = 0xbf2b1680
 [m3video]  8070: SYSTEM: ListElem Shared Addr = 0xbf272280
 [m3vpss ]  8082: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_21] in region 0 ...
 [c6xdsp ]  5557: SYSTEM  : FREE SPACE : System Heap      = 10268448 B, Mbx = 10240 msgs)
 [m3video]  8083: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_24] in region 0 ...
 [m3vpss ]  8082: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_21] in region 0 ...
 [m3video]  8083: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_24] in region 0 ...
 [m3vpss ]  8082: SYSTEM: ListElem Shared Addr = 0xbf2d1080
 [c6xdsp ]  5432: SYSTEM  : Initializing Links ... DONE !!!
 [m3video]  8083: SYSTEM: ListElem Shared Addr = 0xbf2f0a80
 [m3vpss ]  8084: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37
 [m3video]  8085: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_25] in region 0 ...
 [m3vpss ]  8084: SYSTEM  : FVID2 Init in progress !!!
 [c6xdsp ]  5432: SYSTEM  : System DSP Init Done !!!
 [m3video]  8086: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_25] in region 0 ...
 [m3vpss ]  8160: SYSTEM  : FVID2 Init in progress DONE !!!
 [m3video]  8086: SYSTEM: ListElem Shared Addr = 0xbf30e580
 [m3vpss ]  8160: SYSTEM  : Device Init in progress !!!
 [m3video]  8087: HDVICP: Doing PRCM for IVAHD[0] ...
 [m3video]  8087: HDVICP: PRCM for IVAHD[0] ... DONE.
 [m3vpss ] initPrms.isI2cInitReq = 0
 [m3video]  8088: HDVICP: Doing PRCM for IVAHD[1] ...
 [m3video]  8088: HDVICP: PRCM for IVAHD[1] ... DONE.
 [m3vpss ] initPrms.isI2cInitReq = 0
 [m3video]  8088: HDVICP: Doing PRCM for IVAHD[2] ...
 [m3vpss ]  8163: SYSTEM  : Device Init in progress DONE !!!
 [m3video]  8088: HDVICP: PRCM for IVAHD[2] ... DONE.
 [m3vpss ]  8281: SYSTEM  : System VPSS Init Done !!!
 [m3video]  8088: SYSTEM  : Initializing Links !!!
 [m3vpss ]  8281: UTILS: DMA: HWI Create for INT63 !!!
 [m3vpss ]  8281: SYSTEM  : Initializing Links !!!
 [m3video]  8088: SYSTEM  : FREE SPACE : System Heap      = 6280232 B, Mbx = 10240 msgs)
 [m3vpss ]  8281: SYSTEM  : FREE SPACE : System Heap      = 13056 B, Mbx = 10240 msgs)
 [m3video]  8088: SYSTEM  : FREE SPACE : SR0 Heap         = 13452672 B (12 MB)
 [m3vpss ]  8282: SYSTEM  : FREE SPACE : SR0 Heap         = 13452672 B (12 MB)
 [m3video]  8089: SYSTEM  : FREE SPACE : Frame Buffer     = 245104512 B (233 MB)
 [m3vpss ]  8282: SYSTEM  : FREE SPACE : Frame Buffer     = 240794496 B (229 MB)
 [m3video]  8089: SYSTEM  : FREE SPACE : Bitstream Buffer = 218103680 B (207 MB)
 [m3vpss ]  8282: SYSTEM  : FREE SPACE : Bitstream Buffer = 218103680 B (207 MB)
 [m3video]  8089: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 [m3video]  8089: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134217728 B (128 MB)  - TILER ON
 [m3vpss ]  8282: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134217728 B (128 MB)  - TILER ON
 [m3vpss ] Received character 's'
 [m3video]  8090: SYSTEM  : FREE SPACE : Tiler 16-bit     = 134217728 B (128 MB)  [module] vpss probe done.
- TILER ON
 [m3vpss ]  8282: SYSTEM  : FREE SPACE : Tiler 16-bit     = 134217728 B (128 MB)  - TILER ON
 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf005020
 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040
 [m3video] Received character 's'
 [m3video]  8121: SYSTEM  : Initializing Links ... DONE !!!
 [m3vpss ]  8392: SYSTEM  : Initializing Links ... DONE[module] ti81xxfb probe done.
 !!!
 [m3vpss ]  8392: SYSTEM  : Set Static L3 pressure for HDVPSS as High
 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf005020
 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040
 [c6xdsp ] Received character 's'
/opHDMI W1 rev 2.0
t/dvr_rdk/ti816x
[module] ti81xx_hdmi probe done.
 
 ORG 0x46c00524: 0
 NEW 0x46c00524: 2
 it seems everything is ok!!
root@dm816x:/opt/dvr_rdk/ti816x# ./run.sh

 =========
 Main Menu
 =========

 1: VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 2: VCAP + VENC        + VDIS  - SD Encode ONLY
 3: VCAP + VENC        + VDIS  - HD Encode ONLY
 4:               VDEC + VDIS  - SD/HD Decode ONLY
 5: VCAP               + VDIS  - NO Encode or Decode

 e: Exit

 Enter Choice: 5
--------------- CHANNEL DETAILS-------------
Capture Channels => 16
Disp Channels => 16
-------------------------------------------
 0: SYSTEM: System Common Init in progress !!!
 0: SYSTEM: IPC init in progress !!!
 12: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 13: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
 14: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
 16: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
 16: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
 17: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 17: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 18: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 18: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 18: SYSTEM: IPC init DONE !!!
 20: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
 22: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
 23: SYSTEM: ListElem Shared Addr = 0x2b1d2080
 24: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
 26: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
 27: SYSTEM: ListElem Shared Addr = 0x2b1efb80
 28: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
 30: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
 32: SYSTEM: ListElem Shared Addr = 0x2b20d680
 33: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
 35: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
 36: SYSTEM: ListElem Shared Addr = 0x2b22d080
 37: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
 39: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
 41: SYSTEM: ListElem Shared Addr = 0x2b24ca80
 57: SYSTEM: System Common Init Done !!!
 [FBDEV]
 [FBDEV] FB: Starting !!!
 [FBDEV] FB: Opened device [/dev/fb0] (fd=22) !!!
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 2560
 [FBDEV] Physical Address = 8ec00000
 [FBDEV] Buffer Length = 8294400
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 1280
 [FBDEV] Yres - 720
 [FBDEV] Xres Virtual - 1280
 [FBDEV] Yres Virtual - 720
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 6734
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 1843200 Bytes !!!
 [FBDEV]
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 2560
 [FBDEV] Physical Address = 8ec00000
 [FBDEV] Buffer Length = 8294400
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 1280
 [FBDEV] Yres - 720
 [FBDEV] Xres Virtual - 1280
 [FBDEV] Yres Virtual - 720
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 6734
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 1843200 Bytes !!!
 [FBDEV]
 [FBDEV] grpx_fb_draw ...
 [FBDEV] grpx_fb_draw ... Done !!!
 [FBDEV] FB: Start DONE !!!
 [FBDEV]
 189: MCFW  : CPU Revision [ES2.0] !!!
 189: MCFW  : Detected [UNKNOWN] Board !!!  mybe EVM ??
 189: MCFW  : Base Board Revision [REV A] !!! 
 VCAP: TVP5158-0 (0x58): Device not found !!!

 Audio Channels are not supported
 VCAP: TVP5158-1 (0x5c):  NO Video Detected !!!

 Audio Channels are not supported
 VCAP: TVP5158-2 (0x5a): Device not found !!!

 Audio Channels are not supported
 VCAP: TVP5158-3 (0x5e): Device not found !!!

why not found and NO Video Detected  ? all connection is right

 Audio Channels are not supported
 TVP5158: 0x5c: Downloading patch ...
 TVP5158: 0x5c: Downloading patch ... DONE !!!
 TVP5158: 0x5c: 0000:0080:3220
 [m3vpss ]  62251: CAPTURE: Create in progress !!!
 [m3vpss ]  62281: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
 [m3vpss ]  62366: CAPTURE: VIP0 PortB capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
 [m3vpss ]  62451: CAPTURE: VIP1 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
 [m3vpss ]  62537: CAPTURE: VIP1 PortB capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
 [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 58 (58)
 [m3vpss ] CAPTURE::HEAPID:0    USED:992
 [m3vpss ] CAPTURE::HEAPID:4    USED:78759936
 [m3vpss ]  62623: CAPTURE: Create Done !!!
 [m3vpss ]  62623: NSF: Create in progress !!!
 [m3vpss ] NSF::HEAPID:0        USED:128
 [m3vpss ] NSF::HEAPID:1        USED:26048
 [m3vpss ] NSF::HEAPID:4        USED:31653888
 [m3vpss ]  62769: NSF: Create Done !!!
 [m3vpss ]  62770: DEI    : Create in progress !!!
 [m3vpss ]  62951: DEI     : Loading Up-scaling Co-effs
 [m3vpss ]  62951: DEI     : Co-effs Loading ... DONE !!!
 [m3vpss ] DEI:HEAPID:0 USED:64
 [m3vpss ] DEI:HEAPID:1 USED:17088
 [m3vpss ] DEI:HEAPID:4 USED:38737920
 [m3vpss ]  62951: DEI    : Create Done !!!
 [m3vpss ]  62952: DEI    : Create in progress !!!
 [m3vpss ]  63132: DEI     : Loading Up-scaling Co-effs
 [m3vpss ]  63133: DEI     : Co-effs Loading ... DONE !!!
 [m3vpss ] DEI:HEAPID:0 USED:64
 [m3vpss ] DEI:HEAPID:1 USED:16064
 [m3vpss ] DEI:HEAPID:4 USED:38737920
 [m3vpss ]  63133: DEI    : Create Done !!!
 [m3vpss ]  63133: NULL_SRC: Create in progress !!!
 [m3vpss ]  63140: NULL_SRC: Create Done !!!
 [m3vpss ]  63141: MERGE   : Create Done !!!
 [m3vpss ]  63146: DUP   : Create Done !!!
 [m3vpss ]  63147: SWMS: Create in progress !!!
 [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 59 (59)
 [m3vpss ] SWMS: instance 0, sc id 5, start win 0 end win 17
 [m3vpss ]  63248: SWMS0    : Loading Vertical Co-effs (UPSCALE)x ...
 [m3vpss ]  63248: SWMS0    : Loading Horizontal Co-effs (UPSCALE)x ...
 [m3vpss ]  63248: SWMS    : Co-effs Loading ... DONE !!!
 [m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[0]
 [m3vpss ]  63249: SWMS    : ******* Configuring clock 30 secs...
 [m3vpss ]  63249: SWMS0    : Loading Vertical Co-effs (UPSCALE)x ...
 [m3vpss ]  63249: SWMS0    : Loading Horizontal Co-effs (UPSCALE)x ...
 [m3vpss ]  63249: SWMS    : Co-effs Loading ... DONE !!!
 [m3vpss ] 
 [m3vpss ]  *** [SWMS0] Mosaic Parameters ***
 [m3vpss ] 
 [m3vpss ]  Output FPS: 30
 [m3vpss ] 
 [m3vpss ]  Win | Ch  | Input      | Input          | Input         | Input       | Output     |  Output         | Output        | Output      | Low Cost | SWMS | Data  | Blank |
 [m3vpss ]  Num | Num | Start X, Y | Width x Height | Pitch Y / C   | Memory Type | Start X, Y |  Width x Height | Pitch Y / C   | Memory Type | ON / OFF | Inst | Format| Frame |
 [m3vpss ]  ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
 [m3vpss ]    0 |   0 |    0,    0 |   720 x    480 |   720 /   720 | NON-TILED   |    0,    0 |  1920 x   1080 |  3840 /      0 | NON-TILED   |      OFF |    0 |  420SP |   OFF |
 [m3vpss ] 
 [m3vpss ] SWMS:HEAPID:0        USED:360
 [m3vpss ] SWMS:HEAPID:1        USED:47296
 [m3vpss ] SWMS:HEAPID:4        USED:20736000
 [m3vpss ]  63250: SWMS: Create Done !!!
 [m3vpss ]  63251: SWMS: Create in progress !!!
 [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 60 (60)
 [m3vpss ] SWMS: instance 0, sc id 5, start win 0 end win 17
 [m3vpss ]  63352: SWMS1    : Loading Vertical Co-effs (UPSCALE)x ...
 [m3vpss ]  63352: SWMS1    : Loading Horizontal Co-effs (UPSCALE)x ...
 [m3vpss ]  63352: SWMS    : Co-effs Loading ... DONE !!!
 [m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[1]
 [m3vpss ]  63353: SWMS    : ******* Configuring clock 30 secs...
 [m3vpss ]  63353: SWMS1    : Loading Vertical Co-effs (UPSCALE)x ...
 [m3vpss ]  63353: SWMS1    : Loading Horizontal Co-effs (UPSCALE)x ...
 [m3vpss ]  63353: SWMS    : Co-effs Loading ... DONE !!!
 [m3vpss ] 
 [m3vpss ]  *** [SWMS1] Mosaic Parameters ***
 [m3vpss ] 
 [m3vpss ]  Output FPS: 30
 [m3vpss ] 
 [m3vpss ]  Win | Ch  | Input      | Input          | Input         | Input       | Output     |  Output         | Output        | Output      | Low Cost | SWMS | Data  | Blank |
 [m3vpss ]  Num | Num | Start X, Y | Width x Height | Pitch Y / C   | Memory Type | Start X, Y |  Width x Height | Pitch Y / C   | Memory Type | ON / OFF | Inst | Format| Frame |
 [m3vpss ]  ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
 [m3vpss ]    0 |   0 |    0,    0 |   720 x    480 |   720 /   720 | NON-TILED   |    0,    0 |  1920 x   1080 |  3840 /      0 | NON-TILED   |      OFF |    0 |  420SP |   OFF |
 [m3vpss ] 
 [m3vpss ] SWMS:HEAPID:0        USED:360
 [m3vpss ] SWMS:HEAPID:1        USED:43776
 [m3vpss ] SWMS:HEAPID:4        USED:20736000
 [m3vpss ]  63354: SWMS: Create Done !!!
 [m3vpss ]  63354: DISPLAY: Create in progress !!!
 [m3vpss ]  63355: DISPLAY: Create Done !!!
 [m3vpss ]  63356: DISPLAY: Create in progress !!!
 [m3vpss ]  63356: DISPLAY: Create Done !!!
 [m3vpss ]  63358: DISPLAY: Start in progress !!!
 [m3vpss ]  63394: DISPLAY: Start Done !!!
 [m3vpss ]  63394: DISPLAY: HDDAC(BP0) : 57 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!
 [m3vpss ]  63394: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 1, HDDAC(BP0) 1, DVO2(BP1) 1, SDDAC(SEC1) 0
 [m3vpss ]  63394: SYSTEM  : FREE SPACE : System Heap      = 5224 B, Mbx = 10238 msgs)
 [m3vpss ]  63394: SYSTEM  : FREE SPACE : SR0 Heap         = 11003648 B (10 MB)
 [m3vpss ]  63395: SYSTEM  : FREE SPACE : Frame Buffer     = 10769280 B (10 MB)
 [m3vpss ]  63395: SYSTEM  : FREE SPACE : Bitstream Buffer = 218103680 B (207 MB)
 [m3vpss ]  63395: DISPLAY: Start in progress !!!
 [m3vpss ]  63395: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134217728 B (128 MB)  - TILER ON
 [m3vpss ]  63396: SYSTEM  : FREE SPACE : Tiler 16-bit     = 134217728 B (128 MB)  - TILER ON
 [m3vpss ]  63458: DISPLAY: Start Done !!!
 [m3vpss ]  63459: DISPLAY: DVO2(BP1)  : 31 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!
 [m3vpss ]  63459: SWMS: Start in Progress !!!
 [m3vpss ]  63459: SWMS: Start Done !!!
 [m3vpss ]  63459: SWMS: Start in Progress !!!
 [m3vpss ]  63459: SWMS: Start Done !!!
 [m3vpss ]  63501: NULL_SRC: Start Done !!!
 [m3vpss ]  63502: CAPTURE: Start in progress !!!
 [m3vpss ]  63502: CAPTURE: Start Done !!!

 =============
 Run-Time Menu
 =============

 1: Capture Settings
 2: Encode  Settings
 3: Decode  Settings
 4: Display Settings
 5: Audio   Capture / Playback Settings

 6: Audio Capture <TVP5158> & Encode <AAC-LC> demo
 7: Audio encode demo <AAC-LC File In/Out>
 8: Audio decode demo <AAC-LC File In/Out>

 i: Print detailed system information
 s: Core Status: Active/In-active
 f: Switch IVA Channel Map

 e: Stop Demo

 Enter Choice: 

NO Video display on any sreen 。why ?  thanks