Hi all,
we have a strange effect with a c6678 board, xds560v2, and CCS5.3: When the system is powered up and started the first time, everything goes fine. Then I stop the system and do a system reset (from the CCS 'Run' menu) before restart (otherwise the PCIE system will not start correctly). Now, after loading and starting the program again, the system performance is about 10 times slower than before. The pure software function is correct, but it is slow. To get back to the full speed, I have to power-cycle the DSP board and reconnect the debugger etc... which is quite time consuming.
This behaviour is the same on the EVM6678 and our own board based on the EVM. It is also the same for the Linux and Windows versions of CCS5.3 and previous versions back to about 5.1 (earlier version not tested). Moreover, the effect does neither depend on the DSP program nor on the configuration (debug/release); I have the impression it is somehow related to the system reset. We have connected the xds560v2 via USB. I have not tested if the problem also occurs with an xds100.
Has anybody made the same observations?
Thanks, Marcus