Hello,
We had the software built on Rev2.0 on this processor and we were able to toggle GPIO7[15] just fine, but on the new revision Rev2.1 it stays high all the time. The default settings are set in SYSCFG1->PUPDENA and PUPDSEL all enabled, CP[26]-CP[28] set as pull low. We are using the same code to toggle GPIO7[14], GPIO7[13], GPIO7[12] which toggles fine on those pins in Rev2.0 and Rev2.1. There is nothing else connected on this pin at the moment. Any idea why is this happening? This pin was meant for enabling a multiplexer chip on our boards which was disconnected to prove the problem. The problems is the same on 3 more boards using Rev2.1. XJTAG tests on bare PCB board said there are no short-circuits for this track to the 3V3 line. The environment is Code Composer Studio 5.3 and used StarterWare 1.20.03.03 to toggle it.
Best regards,
David.