This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building root filesystem from scratch

Other Parts Discussed in Thread: OMAP-L138

Hi,

Hoping these are quick ones. I am working with an OMAP-L138  running Linux on the ARM. Looking for answers to the following. I remember seeing them somewhere in some document, but can't find it now.

1. How do I build a root file system from scratch for OMAP-L138? I see two tgz in ti-dvsdk_omapl138-evm_04_03_00_06/filesystem folder

arago-base-tisdk-image-da850-omapl138-evm.tar.gz
dvsdk-da850-omapl138-evm-rootfs.tar.gz

Is one a super set of the other? In any case, if you can point me to instruction how to build one from scratch for OMAP-L138,  that will be great. I probably need a set of applications pulled in which is not available in any pre-built packages

2. What is the process to write kernel and root file system to SPI flash and do a boot from everything in flash? I see some instructions at

http://processors.wiki.ti.com/index.php/Booting_Linux_kernel_using_U-Boot#SPI_Flash

Is that the way to do it? i.e. write u-boot scripts to do this. I do not see a way to create partitions in the pre-built u-boot for SPI. Also, the instructions at this link talk about ramdisk. Is it referring only to initrd?

I am hoping that I have posted in the right forum. If not, can you please let me know which forum I should post to?

Cheers,

-raja.