Hello
I just received the 5515EVM. The stethoscope project does not compile.
There are 2 directories for bios in the installed directory:
bios_5_41_02_14 and bios_6_21_00_13
What is the difference between these 2 directories?
Why is there 2 directories and not one?
Which one should be indicated in the include option of the stethoscope project?
Best regards
Michel