This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL137EVM (MVL5) AIC3x Device Driver on which McASPx

Hi Team,

Is there a way to check which McASP0/1/2 was selected at the menu config during the kernel built of the ALSA for SoC Audio Support?

Regards,

Ping

  • Hi Ping,

                To check which McASP (0/1/2) is connected when we enable the ALSA support in kernel config you can look at the kernel source code arch/arm/mach-davinci/board-x.c.

    For example you can look at the DaVinci-PSP-SDK-03.22.00.02/src/kernel/linux-03.22.00.02/arch/arm/mach-davinci/board-da830-evm.c file.

    Regards,

    Iyshwarya

    If this answers your question, please click the Verify Answer button below. If not, please reply back with more information.