Other Parts Discussed in Thread: AM3505
Hello,
I am in the process of bringing-up/debugging a new design which contains a AM3505. I'm experiencing a number of difficulties programming either the NAND Flash or the SDRAM using the Flash tool (v1.6). To that end, I am examining each block of my design in-turn.
For the SDRAM (a 2Gbit Micron MT47H128M16RT), we pin swapped the data bus between the processor and the SRAM to aid routing - we only swapped within byte lanes as follows:
SDRAM Processor
- D0 D5
- D1 D6
- D2 D4
- D3 D1
- D4 D2
- D5 D0
- D6 D3
- D7 D7
- D8 D15
- D9 D12
- D10 D13
- D11 D8
- D12 D11
- D13 D10
- D14 D9
- D15 D14
I can't think of any reason why this would cause a problem, but as I'm having difficulties I'm just covering all my bases.
Can someone confirm that swapping these pins is acceptable - or not?
Thank you,
Kevin Taberski