I need to integrate AAC LC codec with dvsdk for dm6467 board. Is there a specific aac lc encoder for dm6467 board ??
Where should i look for this codec ? If anyone knows, please provide link..
Is the same codec on dm365 compatible with dm6467 ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to integrate AAC LC codec with dvsdk for dm6467 board. Is there a specific aac lc encoder for dm6467 board ??
Where should i look for this codec ? If anyone knows, please provide link..
Is the same codec on dm365 compatible with dm6467 ??
Hi Prateek,
You can download AAC LC encoder for DM6467 from
http://software-dl.ti.com/dsps/dsps_public_sw/codecs/C64XPlus_Audio/index_FDS.html
On DM365, audio codecs run on ARM hence they are not compatible.
Ram
Thanks Ram for the information..
I have tried to download the codec from the link u provided http://software-dl.ti.com/dsps/dsps_public_sw/codecs/C64XPlus_Audio/index_FDS.html.
But still I am not able to download it. The page stuck there and didn't prompt for any download.
HI Ram,
I do have my.TI login but still it is not going further to download page.
I got the following link on my mail
Your download will be available from:
https://focus-webapps.ti.com/licreg/productdownload.tsp?toPerform=productDownload&downloadPage=true&location=http%3A%2F%2Fdownloads.ti.com%2Fdownloads%2Fdsps%2Fdsps_public_sw%2Fcodecs%2FC64XPlus_Audio%2Fc64xplus_aaclcenc_1_20_005_production.bin%3F__gda__%3D1363840473_d68bbdd979a1c55bef9cdabf9841b0cb
-Pratik