I guess the Maintenance packets from the external PE (processing element) can only access to the CSR/CAR Registers in the KeyStone Device.
If the Config_offset field is 0000h, is the REVISION_REG (1000h) accessed or is the DEV_ID (B000h) accessed?
If it is the REVISION_REG (1000h), does an error occur?
For the SRIO Registers does the Config_offset field specify "SRIO Register Offset minus 1000h"?
For example, if the Config_offset field is A060h, the BASE_ID (B060h) is accessed.
Best regards,
Daisuke